×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109476988, Entry date: 07/28/2015
(0)
Rate

How do I transfer data from WinCC Runtime Professional with the help of IndustrialDataBridge?

  • Entry
  • Associated product(s)
Find out, how you can use the WinCC IndustrialDataBridge option also in combination with WinCC Runtime Professional.
The WinCC IndustrialDataBridge option makes it possible to read out data from the WinCC Runtime Professional  and to provide it to other programs with the help of various interfaces, for example, for the archiving of process values in a database.
  

Figure 01
 
Download
In the documentation you can find a description of how to configure WinCC Runtime Professional and the IndustrialDataBridge in order to enable the transmission of data.
  Documentation_en.pdf (1,6 MB)

Additional Information
Basic information about IndustrialDataBridge, such as, for example, the types of different interfaces can be found in the following entries:

  • Manual
    SIMATIC HMI WinCC V7.2 WinCC/IndustrialDataBridge
    Entry ID: 73968329
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.