×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109477299, Entry date: 06/09/2015
(0)
Rate

Soft Starter 3RW44 PCS 7 Library V6.2 / V7.1 Update

  • Entry
  • Associated product(s)
The Soft Starter 3RW44 PCS 7 Library V6.2 / V7.1 Update is available for download.

Software requirements:

For V6.2:
The library requires as a minimum SIMATIC PCS 7 V6.1 SP4.
The Soft Starter ES Professional software is necessary to be able to integrate 3RW44 as an S7 slave.

For V7.1:
The library requires as a minimum SIMATIC PCS 7 V7.0 or SIMATIC PCS 7 V7.1.
The Soft Starter ES Professional software is necessary to be able to integrate 3RW44 as an S7 slave.

Hardware requirements:

Please refer to the „Readme“ file.
  Readme_V6.2-7.1.zip (53,5 KB)


What is new in V6.2 / V7.1?

The following new functions are supported in PCS 7 Soft Starter 3RW44 V6.2 / V7.1 compared to V6.1+SP2 / V7.0+SP2:

  • Logbook data reading in SS_DIR has been made acyclic. User can read Logbook data by using Read data command from faceplate/ CFC function block. “Refresh” button in Logbook is replaced with “Readdata” button.
  • Incorrect reading of “LOGTIME5” value in Logbook has been corrected.
  • Diagnostic data of SS_DIAG has been made acyclic. Diagnostic data is updated through interrupts and the user can also read diagnostic data by using Read data command from SS_DIR Diagnostic views/ SS_MEAS Diagnostic views/ function block.
  • A Read data button has been added in the following views to facilitate acyclic diagnostics data reading:
    • Control Diagnostics View (SS_DIR)
    • Device Diagnostics View (SS_DIR)
    • Parameter Diagnostics View (SS_DIR)
    • Measurement Diagnostics View (SS_MEAS)
  • Opening of faceplate views of SS_DIR/SS_STAT/SS_MEAS through “tag point by tag” option at WINCC RT (SR= 1-3754538844) has been made available.
  • "Order Number" text in Readme has been replaced with "Article Number”
  • Module driver support for 3RW4423-*BC** (OM configuration) has been included.
  • Module driver support for Soft Starter EDD V2.0 with GSD SI0180DE.GS? has been included.
  • WINCC RT crash upon opening Logbook faceplate view has been fixed.
  • On generation of Rack Fault or Module fault, the control buttons at the SS_DIR,SS_STAT,SS_MEAS are disabled at WinCC RT.

Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the ReadMe_OSS_V6.2 and ReadMe_OSS_V7.1 file.

Special information for resellers

The information and the license terms in the ReadMe_OSS_V6.2 and ReadMe_OSS_V7.1 file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

  ReadMe_OSS_V6.2.rtf (156,2 KB)
  ReadMe_OSS_V7.1.rtf (156,3 KB)

 
Download:

 Download unterliegt Exportcontrolle  PCS7_Soft_Starter_3RW44_V6.2_V7.1.zip (152,9 MB)
Note: The software is subject to export restrictions. The download is only available to registered users

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.