×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109477641, Entry date: 08/23/2018
(21)
Rate

SINAMICS S120 (S150, G130, G150): SINAMICS Support Package SSP

  • Entry
  • Associated product(s)
Here you will find the SINAMICS Support Packages (SSP) for SINAMCIS S120 that matches STARTER or SCOUT


Actual SINAMICS MICROMASTER STARTER

You can download the actual STARTER here: 26233208 


SSP SINAMICS S120 V5.2 HF2 (S150, G130, G150)

The original SSP SINAMICS S120 V5.2 / V5.2 HF1 is replaced with the SSP SINAMICS S120 V5.2 HF2 here. If you already had installed the SSP SINAMICS S120 V5.2 or V5.2 HF1, please install the SSP HF2 at your STARTER/SCOUT environment.
With this SINAMICS Support Package, SINAMICS drives belonging to the SINAMICS S120 series with firmware release V5.2 can be configured and commissioned using STARTER or SCOUT.

OSS note on SSP SINAMICS S120 V5.2 HF2 (S150, G130, G150)

Third-party software - license conditions and copyright notes
You can find the copyright notes on the third-party software, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the following file:
SSP_SINAMICS_V5_2_HF2.zip/SSP_SINAMICS_V5_2/02_OSS_Information/ReadMe_OSS.zip

Special note for resellers
The information and the license conditions in the ReadMe_OSS.zip file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

Availability OSS Source Code
Some license conditions of third-party software components used in this product may oblige us to provide you with the source text and further information for these components. You can find this information in the file SSP_SINAMICS_V5_2_HF2.zip (at the folder ...\SSP_SINAMICS_V5_2\02_OSS_Information\Open_Source_Software.zip).

SSPs for updating existing STARTER resp. SCOUT installations
(please read detailed description) 

SSP installation at "SCOUT TIA" not possible!

  installable integrated

SSP, SINAMICS S120 V5.2 HF2

 Registrierung notwendig  SSP_SINAMICS_V5_2_HF2.zip (32,9 MB)

SHA-512 checksum:

 Registrierung notwendig  sha512zip_SINAMICS_V5_2_HF2.txt (1 KB)

Information about SHA-512: 109483101

STARTER
from V5.1 SP1 HF2

SCOUT from
V5.2 SP1

STARTER 
>= V5.3 HF1 

SCOUT 
>= V5.3 SP1

With this SINAMICS Support Package, SINAMICS drives belonging to the SINAMICS S120 series with firmware release V5.2 can be configured and commissioned using STARTER or SCOUT.

Procedure for installing SSP

  1. Download the attached ZIP file
  2. Unzip the ZIP file to a shared target directory on your hard disk.
    Please ensure that there are absolutely no spaces in the complete path names of this target directory.
  3. After unpacking, the shared directory must appear as follow:
    \...\01_Readme\
    \...\02_OSS_Information\
    \...\CD_1\
  4. Start the SSP setup program by calling it from /CD_1/SETUP.EXE.

The readme file contains important notes on how to use the tool.

Note on online help for function release V5.2
With installation of SSP SINAMICS S120 V5.2 HF2 the online help of the STARTER installation itself will not be updated.
Updating this online help is possible with installation of the online help program package SSP SINAMICS HELP V5.2. Download link: 109759443 


SSP SINAMICS S120 V5.1 SP1 HF2 (S150, G130, G150)

The original SSP SINAMICS S120 V5.1 SP1 / V5.1 SP1 HF1 is replaced with the SSP SINAMICS S120 V5.1 SP1 HF2 here.
If you already had installed the SSP SINAMICS S120 V5.1 SP1 or V5.1 SP1 HF1, please install the SSP HF2 at your STARTER/SCOUT environment.
With this SINAMICS Support Package, SINAMICS drives belonging to the SINAMICS S120 series with firmware release V5.1 SP1 can be configured and commissioned using STARTER or SCOUT.

OSS note on SSP SINAMICS S120 V5.1 SP1 HF2 (S150, G130, G150)

Third-party software - license conditions and copyright notes
You can find the copyright notes on the third-party software, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the following file:
SSP_SINAMICS_V5_1_SP1_HF2.zip/SSP_SINAMICS_V5_1_SP1/02_OSS_Information/ReadMe_OSS.zip

Special note for resellers
The information and the license conditions in the ReadMe_OSS.zip file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

Availability OSS Source Code
Some license conditions of third-party software components used in this product may oblige us to provide you with the source text and further information for these components. You can find this information in the file SSP_SINAMICS_V5_1_SP1_HF2.zip (at the folder ...\SSP_SINAMICS_V5_1_SP1\02_OSS_Information\Open_Source_Software.zip).


SSPs for updating existing STARTER resp. SCOUT installations
(please read detailed description) 

SSP installation at "SCOUT TIA" not possible!

  installable integrated

SSP, SINAMICS S120 V5.1 SP1 HF2

 Registrierung notwendig  SSP_SINAMICS_V5_1_SP1_HF2.zip (32,5 MB)

SHA-512 checksum:

 Registrierung notwendig  sha512zip_SINAMICS_V5_1_1_HF2.txt (1 KB)

Information about SHA-512: 109483101

STARTER
from V4.5 SP1

SCOUT from
V4.5

STARTER 
> V5.3 HF1 

SCOUT 
>= V5.3 SP1

With this SINAMICS Support Package, SINAMICS drives belonging to the SINAMICS S120 series with firmware release V5.1 SP1 can be configured and commissioned using STARTER or SCOUT.

Procedure for installing SSP

  1. Download the attached ZIP file
  2. Unzip the ZIP file to a shared target directory on your hard disk.
    Please ensure that there are absolutely no spaces in the complete path names of this target directory.
  3. After unpacking, the shared directory must appear as follow:
    \...\01_Readme\
    \...\02_OSS_Information\
    \...\CD_1\
  4. Start the SSP setup program by calling it from /CD_1/SETUP.EXE.

The readme file contains important notes on how to use the tool.

Note on online help for function release V5.1 SP1
With installation of SSP SINAMICS S120 V5.1 SP1 HF2 the online help of the STARTER installation itself will not be updated.
Updating this online help is possible with installation of the online help program package SSP SINAMICS HELP V5.1 SP1. Download link: 109759443

SSP SINAMICS S120 V5.1 HF3 (S150, G130, G150)

The original SSP SINAMICS S120 V5.1 HF2 is replaced with the SSP SINAMICS S120 V5.1 HF3 here.
If you already had installed the SSP SINAMICS S120 V5.1 or HF1 or HF2, please install the SSP HF3 at your STARTER/SCOUT environment.
With this SINAMICS Support Package, SINAMICS drives belonging to the SINAMICS S120 series with firmware release V5.1 can be configured and commissioned using STARTER or SCOUT.

OSS note on SSP SINAMICS S120 V5.1 HF3 (S150, G130, G150)

Third-party software - license conditions and copyright notes
You can find the copyright notes on the third-party software, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the following file:
SSP_SINAMICS_V5_1_HF3.zip/SSP_SINAMICS_V5_1/02_OSS_Information/ReadMe_OSS.zip

Special note for resellers
The information and the license conditions in the ReadMe_OSS.zip file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

Availability OSS Source Code
Some license conditions of third-party software components used in this product may oblige us to provide you with the source text and further information for these components. You can find this information in the file SSP_SINAMICS_V5_1_HF3.zip (at the folder ...\SSP_SINAMICS_V5_1\02_OSS_Information\Open_Source_Software.zip).

SSPs for updating existing STARTER resp. SCOUT installations
(please read detailed description) 

SSP installation at "SCOUT TIA" not possible!

  installable integrated

SSP, SINAMICS S120 V5.1 HF3

 Registrierung notwendig  SSP_SINAMICS_V5_1_HF3.zip (32,4 MB)

SHA-512 checksum:

 Registrierung notwendig  sha512zip_SINAMICS_V5_1_HF3.txt (1 KB)

Information about SHA-512: 109483101

STARTER
from V4.5 SP1

SCOUT from V4.5

STARTER 
>= V5.3 HF3 

SCOUT 
> V5.3 SP1

With this SINAMICS Support Package, SINAMICS drives belonging to the SINAMICS S120 series with firmware release V5.1 can be configured and commissioned using STARTER or SCOUT.

Procedure for installing SSP

  1. Download the attached ZIP file
  2. Unzip the ZIP file to a shared target directory on your hard disk.
    Please ensure that there are absolutely no spaces in the complete path names of this target directory.
  3. After unpacking, the shared directory must appear as follow:
    \...\01_Readme\
    \...\02_OSS_Information\
    \...\CD_1\
  4. Start the SSP setup program by calling it from /CD_1/SETUP.EXE.

The readme file contains important notes on how to use the tool.

Note on online help for function release V5.1
With installation of SSP SINAMICS S120 V5.1 HF3 the online help of the STARTER installation itself will not be updated.
Updating this online help is possible with installation of the online help program package of the tool STARTER V5.1 SP1.


SSP SINAMICS S120 V4.8 HF2 (S150, G130, G150)

The original SSP SINAMICS S120 V4.8 HF1 is replaced with the SSP SINAMICS S120 V4.8 HF2 here.
If you already had installed the SSP SINAMICS S120 V4.8 or HF1, please install the SSP HF2 at your STARTER/SCOUT environment. With this SSP HF2 the new S120 S120 Motor Modules Booksize C-/D-Type 24 A, 45 A, 60 A (ID: 109751266) at STARTER/SCOUT are available.

OSS note on SSP SINAMICS S120 V4.8 HF2 (S150, G130, G150)

Third-party software - license conditions and copyright notes
You can find the copyright notes on the third-party software, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the following file:

  ReadMe_OSS.zip (21,0 KB)

Special note for resellers
The information and the license conditions in the ReadMe_OSS.htm file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

Availability OSS Source Code
Some license conditions of third-party software components used in this product may oblige us to provide you with the source text and further information for these components. You can find this information in the file SSP_SINAMICS_V4_8_HF2.zip (at the folder ...\02_OSS_Information\Open_Source_Software.zip).


SSPs for updating existing STARTER resp. SCOUT installations
(please read detailed description) 

SSP installation at "SCOUT TIA" not possible!

  installable integrated

SSP, SINAMICS S120 V4.8 HF2

 Registrierung notwendig  SSP_SINAMICS_V4_8_HF2.zip (31,3 MB)

STARTER
from V4.5 SP1

SCOUT from V4.5

STARTER 
from V5.1 SP1

SCOUT from V5.1

With this SINAMICS Support Package, SINAMICS drives belonging to the SINAMICS S120 series with firmware release V4.8 can be configured and commissioned using STARTER or SCOUT.

Procedure for installing SSP

  1. Download the attached ZIP file
  2. Unzip the ZIP file to a shared target directory on your hard disk.
    Please ensure that there are absolutely no spaces in the complete path names of this target directory.
  3. After unpacking, the shared directory must appear as follow:
    \...\01_Readme\
    \...\02_OSS_Information\
    \...\CD_1\
  4. Start the SSP setup program by calling it from /CD_1/SETUP.EXE.

The readme file contains important notes on how to use the tool.

Note on online help for function release V4.8
With installation of SSP SINAMICS S120 V4.8 the online help of the STARTER installation itself will not be updated.
Updating this online help is possible with installation of the online help program package of the tool STARTER V4.5 SP1.


SSP SINAMICS S120 Hotfix Package V4.7 (S150, G130, G150) for configuration of a PT1000 (RT V4.7 >= HF17) 

SSPs for updating existing STARTER installations
(please read detailed description);

Not for SCOUT Installation!

SSP installation at "SCOUT TIA" not possible!

  installable integrated
Hotfix SSP, SINAMICS S120 V4.7
 Registrierung notwendig  SSP_SINAMICS_HOTFIX_PACKAGE_V4_7.zip (206,1 MB)
STARTER
from V4.4 und < V4.5 SP1
STARTER 
from V4.5 SP1
SCOUT 
from V4.5

With this SINAMICS Support Package (Hotfix), SINAMICS drives belonging to the SINAMICS S120 series with firmware release V4.7 >= HF17 (configuration of a PT1000 possible) can be configured and commissioned using STARTER.
The installation of this Hotfix is recommended if a configuration of PT1000 temperature sensors is required.

Procedure for installing SSP

  1. Download the attached ZIP file
  2. Unzip the ZIP file to a shared target directory on your hard disk.
    Please ensure that there are absolutely no spaces in the complete path names of this target directory.
  3. After unpacking, the shared directory must appear as follow:
    \...\01_Readme\
    \...\CD_1\
  4. Start the SSP setup program by calling it from /CD_1/SETUP.EXE.1)

The readme file contains important notes on how to use the tool.

 

SSP SINAMICS S120 V4.7 (S150, G130, G150) 

SSPs for updating existing STARTER 
(please read detailed description); 

Not for SCOUT Installation!

SSP installation at "SCOUT TIA" not possible!

  installable integrated
SSP, SINAMICS S120 V4.7
 Registrierung notwendig  SSP_SINAMICS_V4_7_update.zip (30,3 MB)
STARTER
from V4.3.2.x
STARTER 
from V4.4 /
SCOUT from V4.4

With this SINAMICS Support Package, SINAMICS drives belonging to the SINAMICS S120 series with firmware release V4.7 can be configured and commissioned using STARTER or SCOUT.

Procedure for installing SSP

  1. Download the attached ZIP file
  2. Unzip the ZIP file to a shared target directory on your hard disk.
    Please ensure that there are absolutely no spaces in the complete path names of this target directory.
  3. After unpacking, the shared directory must appear as follow:
    \...\01_Readme\
    \...\CD_1\
  4. Start the SSP setup program by calling it from /CD_1/SETUP.EXE.1)

The readme file contains important notes on how to use the tool.

Note on online help for function release V4.7
With installation of SSP SINAMICS S120 V4.7 the online help of the STARTER installation itself will not be updated.
Updating this online help is possible with installation of the online help program package of the tool STARTER V4.4.


SSP SINAMICS S120 V4.6 (S150, G130, G150) 

SSPs for updating existing STARTER resp. SCOUT installations
(please read detailed description)

SSP installation at "SCOUT TIA" not possible!

  installableintegrated
SSP, SINAMICS S120 V4.6
 Registrierung notwendig  SSP_SINAMICS_V4_6.zip (26,2 MB)
STARTER 
from V4.3.1.x 

SCOUT 
from V4.3.1.x
STARTER
from V4.3.2.x

SCOUT
from V4.4

With this SINAMICS Support Package, SINAMICS drives belonging to the SINAMICS S120 series with firmware release V4.6 can be configured and commissioned using STARTER or SCOUT.

Procedure for installing SSP

  1. Download the attached ZIP file
  2. Unzip the ZIP file to a shared target directory on your hard disk.
    Please ensure that there are absolutely no spaces in the complete path names of this target directory.
  3. After unpacking, the shared directory must appear as follow:
    \...\01_Readme\
    \...\CD_1\
  4. Start the SSP setup program by calling it from /CD_1/SETUP.EXE.1)

The readme file contains important notes on how to use the tool.

Note on online help for function release V4.7
With installation of SSP SINAMICS S120 V4.7 the online help of the STARTER installation itself will not be updated.
Updating this online help is possible with installation of the online help program package of the tool STARTER V4.4.


SSP SINAMICS S120 Hotfix Package V4.5 (S150, G130, G150) for configuration of a PT1000 (RT V4.5 >= HF31) 

SSPs for updating existing STARTER installations
(please read detailed description);

Not for SCOUT Installation!

SSP installation at "SCOUT TIA" not possible!

  installable integrated
Hotfix SSP, SINAMICS S120 V4.5
 Registrierung notwendig  SSP_SINAMICS_HOTFIX_PACKAGE_V4_5.zip (92,0 MB)
STARTER
from V4.4 und < V4.5 SP1
STARTER 
from V4.5 SP1
SCOUT 
from V4.5

With this SINAMICS Support Package (Hotfix), SINAMICS drives belonging to the SINAMICS S120 series with firmware release V4.5 >= HF31 (configuration of a PT1000 possible) can be configured and commissioned using STARTER.
The installation of this Hotfix is recommended if a configuration of PT1000 temperature sensors is required.

Procedure for installing SSP

  1. Download the attached ZIP file
  2. Unzip the ZIP file to a shared target directory on your hard disk.
    Please ensure that there are absolutely no spaces in the complete path names of this target directory.
  3. After unpacking, the shared directory must appear as follow:
    \...\01_Readme\
    \...\CD_1\
  4. Start the SSP setup program by calling it from /CD_1/SETUP.EXE.1)

The readme file contains important notes on how to use the tool. 

1): Hint according the follow SSP Setup-notice: The SSP can not be installed because of an incorrect Windows operating system.
Please install the SSP via the actual version of the STARTER tool.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.