×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109477754, Entry date: 08/23/2017
(2)
Rate

SINAMICS Brake Test with SINUMERIK 840D sl

  • Entry
  • Associated product(s)
Description
Axes and mechanical systems can drop due to gravity when the drives are switched off. Dangerous motion can result for vertical axes or for rotary axes or spindles with an asymmetrical weight distribution. For this reason, a drive must also be safely held in position when switched off (no current condition). This is usually implemented using a holding brake. The reliability of this holding brake is an essential part of the protection function against falling vertical axes.
The "Safe Brake Control" function (SBC) is used to control holding brakes that function according to the closed-circuit principle (e.g. motor holding brake). The brake is controlled via a two-channel output of the SINAMICS Motor Module. SBC (if configured) is always triggered together with STO.
The brake test checks whether the expected holding torque is still available. The drive moves against the closed brake and applies the test torque – there should be no axis movement if the test is successful. However, if an axis movement is detected, it must be assumed that the brake holding torque is no longer sufficient to hold the axis in position. In this case, the relevant axis must be traversed to a safe position and the brake checked and repaired, if required.

Documentation
  109477754_SINAMICS_Brake_test_V6_en.pdf (2,1 MB)

Programs
 Registrierung notwendig  SI_BT_AWL_V3.0.AWL (15,9 KB) 

Last changes
01/2018

Additonal search terms
motioncontrol_cnc_applications

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.