×
Siemens Industry Online Support
Siemens AG
Entry type: Download, Entry ID: 109477825, Entry date: 04/06/2017
(4)
Rate

Firmware update for CPU 1214 FC, DC/DC/DC, 14DI/10DO/2AI

  • Entry
  • Associated product(s)
Firmware update for CPU 1214 FC, DC/DC/DC, 14DI/10DO/2AI

When updating the operating system, always update to the latest version available for the product and its respective article number. The previous versions of the operating system are only intended as backup to allow a downgrade to the original version. Until now this is not known to have been necessary in any case.

The respective latest version of a CPU operating system is valid for all versions of that article number.

 

Required user action:

You can install the CPU firmware update from the Web server, the online diagnostic functions of STEP 7, or by making an SIMATIC memory card using the Siemens customer support Web site that contains the firmware update. The S7-1200 System Manual documents these methods.

If you use an SIMATIC memory card to install the CPU firmware update, retentive memory is retained. However, if you use the Web server or online diagnostic functions of STEP 7 to install the update, retentive memory is lost.

If you close the Web browser while in the process of performing a firmware update from the Web server, you will be unable to change the operating mode of the CPU to RUN mode. If this situation happens, you must cycle power to the CPU to be able to change the CPU to RUN mode.


Overview of article numbers and firmware versions of the CPU 1214 FC, DC/DC/DC, 14DI/10DO/2AI:
Note: The software is subject to export restrictions, a download is only available to registered users.

 Article number

Firmware
version

Update with ...
 6ES7214-1AF40-0XB0  
 V4.2.1 

Third-party software - Licensing terms and copyright
information

You can find the copyright information for third-party
software contained in this product, particularly open source
software, as well as applicable licensing terms of such
third-party software in the Readme_OSS_V421 file.


Special information for resellers
The information and the license terms in the
Readme_OSS_V421 file must be passed on to the
purchasing party to avoid license infringements by the
reseller or purchasing party. 


 Registrierung notwendig  ReadMe_OSS_V421.htm (749,8 KB)


Recommended for update:

see description update 4.2.1

 Download unterliegt Exportcontrolle  6ES7214-1AF40-0XB0_V04.02.01.zip (9,1 MB)

 V4.2 Backup only:

see description update 4.2

 Download unterliegt Exportcontrolle  6ES7214-1AF40-0XB0_V04.02.00.zip (9,1 MB) 

 V4.1.3

Backup only:

see description update 4.1.3

 Download unterliegt Exportcontrolle  6ES7214-1AF40-0XB0_V04.01.03.zip (9,3 MB)

 V4.1.2 

Backup only:

see description update 4.1.2

 Download unterliegt Exportcontrolle  6ES7214-1AF40-0XB0_V412.zip (9,1 MB)

 V4.1.1

Backup only:

 Download unterliegt Exportcontrolle  6ES7214-1AF40-0XB0_V411.ZIP (9,1 MB)


 Update V4.2.1

 

CPU Firmware update V4.2.1. replaces CPU Firmware update V4.2.0.
CPU Firmware update V4.2.1 makes improvements to several customer-reported areas of functionality. CPU firmware update V4.2.1 allows the S7-1200 CPU to accept a project download from STEP 7 V13 (TIA Portal V13) where the project includes high-speed counters (HSCs).


 Update V4.2


CPU Firmware update V4.2 replaces CPU Firmware update V4.1.3

  • Key features supported by S7-1200 CPU firmware V4.2 include:
  • Control/Monitoring of fail-safe devices on PROFINET IO and PROFIBUS DP
  • Improved CPU execution times
  • Enhancements to the Web server
  • New programming instructions including 2 new basic instructions and 24 extended instructions
  • New communication capabilities
  • Backup and restore of an online S7-1200 CPU and F-CPU from STEP 7
  • New high-speed counter (HSC) capabilities
  • Enhancements to capturing and loading an online DB snapshot
  • Introduced F-CPU to F-CPU communication in CPU firmware V4.2 and STEP 7 Safety Basic V14 or STEP 7
    Safety Advanced V14

The desribed functiuonality requires the software: STEP 7 V14 Basic or Professional.


NOTICE: S7-1200 CPUs with Functional Stand 05 (FS: 05) or later cannot be downgraded to firmware versions prior to

V4.2.0.



 Update V4.1.3

 

 

CPU Firmware update V4.1.3 replaces CPU Firmware update V4.1.2.

S7-1200 FW V4.1.3 allows to execute motion function blocks in any OB.

 

 Update V4.1.2

 Notice:
To ensure proper operation of motion control programs with S7-1200 FW V4.1.2, it must execute all motion function blocks from OB 1 or from blocks that OB 1 calls. To use motion control without this restriction, use FW V4.1.1.
If it isn't used motion control in the project, it can used FW V4.1.2.

S7-1200 CPU Firmware update V4.1.2 improves CPU program execution time of some instructions through targeted instruction optimization.

 

 

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.