×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109478287, Entry date: 07/22/2015
(2)
Rate

SINAMICS S120, CU310-2 PN, CU320-2 PN: Maintenance request when allocating NameOfStation

  • Entry
  • Associated product(s)
Maintenance request when allocating NameOfStation. The MAINT LED of the CPU lights up yellow.

Question:
In STEP 7 HW Config, why is a maintenance request signaled at the CU320-2 PN / CU310-2 PN when allocating NameOfStation?
The MAINT LED of the CPU lights up yellow.

Answer:

Fault status:
In the HW configuration in Step 7, a maintenance request is signaled at the CU320-2 PN/CU310-2 PN.
The message (under details for the diagnostics) is as follows:

A NameOfStation was already configured/allocated for an additional interface of this module, which is identical to what was entered for this interface.

Cause of the error:
CU3x0-2 PN modules have an IE and a PN interface.
Not only must the addresses of the IE (X127) and the PN interface (X150) be different.

Also the name of the X127 (r8910) must be different than the name of the X150 (r8930).

Remedy:
Establish a connection to the interface X127 of the CU, and allocate a different name.

Note:
In this particular case, a multi-interface error is signaled in the TIA Portal.

Examples of errors:


Picture 1

 


Picture 2
 
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.