×
Siemens Industry Online Support
Siemens AG
Type de contribution : Exemple d’application ID de la contribution : 109478439, Date de la contribution : 11/11/2015
(0)
Évaluer

SIMATIC PCS 7 in the pharmaceutical industry “Fermentation” (demo project)

  • Contribution
  • Concerne le/les produits(s)
In this application example, SIMATIC PCS 7 and SIMATIC BATCH are used to depict and control the fermentation process manage with the required high level of efficiency, quality and performance.

Fermentation is the process of cultivating organic materials. This process involves several phases and takes place under strict guidelines and strictly controlled ambient conditions.

The application example is realized as a SIMATIC PCS 7 multiproject in accordance with ISA-88 and provides a template that comprises all typical components, their open- and closed-loop control, the necessary logic and locking as well as the visualization. It is modularly structured and based on standardized equipment and control modules.
 

This application example contains typical equipment modules for controlling a fermentation system, e.g.:

  • Dosing substances
  • Controlling the stirrer
  • Controlling the temperature, the pressure, the airflow rate and the pH values
  • Cleaning the fermenter and transferring the materials

In the application example, the sequence of the entire process is controlled via SIMATIC BATCH.

Advantages
Using the application example has the following advantages:

  • A reduction of the knowledge necessary to develop applications
  • A decrease in the configuration effort
  • More flexible setup and adaptation due to equipment modules
 
Validity
SIMATIC PCS 7 V8.1
SIMATIC BATCH V8.1

Documentation and Project 
  Documentation (1,9 MB)
 Registrierung notwendig  Sample project for PCS 7 V8.1 (183,5 MB)

Further Information
Media system - Pharma Demo Applications
Application example - SIMATIC PCS 7 in the pharmaceutical industry “Blood Plasma Fractionation”
Application example - SIMATIC PCS 7 in the pharmaceutical industry “Freeze Dryer”
Application example - PCS 7 Unit Template "CIP - Cleaning in Place"
Application example - Equipment Modules for PCS 7 using the example of the Chemical Industry

Notes relatives à la sécurité
La protection des installations, systèmes, machines et réseaux contre les cyber-menaces nécessite la réalisation (et le maintien continu) d'un concept global de sécurité IT à la pointe de la technique. Les produits et solutions Siemens ne constituent qu'un élément d'un tel concept. Pour plus d’informations sur la cyber-sécurité, rendez-vous sur
https://www.siemens.com/cybersecurity#Ouraspiration.
Aide pour la statistique
Cette fonction permet de délivrer les identifiants des résultats de la recherche selon la quantité souhaitée (format .txt).

Générer une liste
Copier l'URL
Afficher cette page dans le nouveau design
Poste de commande mySupport