×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109478440, Entry date: 05/13/2019
(0)
Rate

Firmware update for ET 200SP DI 8x24VDC HIGH SPEED

  • Entry
  • Associated product(s)
Firmware update for ET 200SP DI 8x24VDC HIGH SPEED
Description:

When updating the firmware, always update to the latest version available for the product and its respective article number. The previous versions of the firmware are only intended as backup to allow a downgrade to the original version.
The respective latest version of a firmware is valid for all versions of that article number.

How to update the firmware is described in detail in entry ID 78646133

Note:
If an I/O module is replaced or upgraded by means of a firmware update, the firmware of the interface module may also need to be updated.
The following table shows the interface module versions for which an update is necessary:

Affected
interface module
Article numberMinimum firmware versionRegards supply from
Siemens stock until ca.
IM155-6PN ST (PROFINET)6ES7155-6Ax00-0BN0V1.1.112/2013
IM155-6DP HF (PROFIBUS)6ES7155-6Bx00-0CN0V1.1.012/2013
IM155-6PN HF (PROFINET)6ES7155-6AU00-0CN0 V2.1.012/2013

Therefore, we urgently recommend that you update the firmware of the interface modules listed above for IMs with a firmware version lower than the minimum firmware version.

 

Overview of article numbers and firmware versions of the  ET 200SP DI 8x24VDC HIGH SPEED:

Article number

FW version

Update with...

6ES7131-6BF00-0DA0

  
 V1.0.3

For Upgrade:
For a description, see below Update V1.0.3

For STEP 7 as of Version 5.5
 Registrierung notwendig  Classic_6ES7131-6BF00-0DA0_V103.ZIP (50,1 KB) 
For STEP 7 TIA-Portal
 Registrierung notwendig  TIA_6ES7131-6BF00-0DA0_V103.ZIP (50,1 KB)

 V1.0.2

Backup only:
For a description, see below Update V1.0.2

For STEP 7 as of Version 5.5
 Registrierung notwendig  Classic_6ES7131-6BF00-0DA0_V102.ZIP (50,1 KB)

For STEP 7 TIA-Portal
 Registrierung notwendig  TIA_6ES7131-6BF00-0DA0_V102.ZIP (50,1 KB)

 V1.0.1

Backup only:
For a description, see below Update V1.0.1

For STEP 7 as of Version 5.5
 Registrierung notwendig  Classic_6ES7131-6BF00-0DA0_V101.EXE (168,0 KB)

For STEP 7 TIA-Portal
 Registrierung notwendig  TIA_6ES7131-6BF00-0DA0_V101.EXE (168,0 KB)

 

V1.0.0

Backup only:

For STEP 7 as ofVersion 5.5
 Registrierung notwendig  Classic_6ES7131-6BF00-0DA0_V100.EXE (168,0 KB)

For STEP 7 TIA-Portal
 Registrierung notwendig  TIA_6ES7131-6BF00-0DA0_V100.EXE (168,0 KB)


Update V1.0.3

Firmware adaptation for the operating mode "counting" in combination with the modular cam controller (MCC) of DQ 4x24VDC/2A HS (Firmware V2.0.0 and higher).


Update V1.0.2

Support of a PN clock starting at 125µs, even in isochronous mode.

Increased precision during update of the actual values when process interrupts are triggered in isochronous mode.

Increased precision of the synchronization time point in isochronous mode.

 

Update V1.0.1

Change caused by production

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.