×
Siemens Industry Online Support
Siemens AG
文档类型 应用与工具 文档编号 109478514, 文档发布日期 2015年10月22日
(4)
评估

Sample project for the PROFINET Driver for Controller

  • 文档
  • 涉及产品
This application example shows you how to implement a PROFINET controller on a standard PC using the PN Driver for Controller.

Solution
This application example shows you how to create an executable PN controller with the aid of the PN Driver C/C++ libraries and an XML hardware configuration generated by TIA Portal. In the example, the controller controls a virtual automatic baking machine that consists of multiple PN devices. The program is implemented as a simple console application.


 

Using the documented source code, the example shows you
 
  • how to control a SINAMICS drive
  • how to read in digital and analog signals of an ET 200SP
  • how to control a PROFINET KP8 PN Key Panel
  • and how to handle alarm and interrupt events

In addition, the documentation includes a user guide that shows all the steps you need to quickly and conveniently create a PROFINET application in Windows. 

Comment
An original PN Driver for Controller is required to run this application.

Documentation and Sample Project 
  PROFINET Driver for Controller (1,1 MB)
 Registrierung notwendig  Project for STEP 7 V12 & C-Source Code (562,5 KB)

 

 

 

安全性信息
为了保护技术基础设施、系统、机器和网络免受网络威胁,有必要实施并持续维护一个全面、最先进的IT安全方案。西门子的产品和解决方案构成了这一方案的一个要素。有关网络安全的更多信息,请访问
https://www.siemens.com/cybersecurity#Ouraspiration.