×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109479024, Entry date: 12/21/2016
(0)
Rate

Updates for SIMOCODE ES V13 SP1 (TIA Portal)

  • Entry
  • Associated product(s)
Available downloads: Overview of the current and earlier versions

Current version

Status December 2016: Update 3

This update is valid for the following product:

  • SIMOCODE ES V13 SP1 (TIA Portal)

In conjunction with PROFINET devices Note the following:

Devices connected to an enterprise network or directly to the internet must be appropriately protected against unauthorized access, e.g. by use of firewalls and network segmentation. For more information about industrial security, please visit  http://www.siemens.com/industrialsecurity 

 Bug-fixing:

  • Even when multiple devices were selected for download only the parameterization of the last device was loaded.

  • A download of a parameterization on to a device could lead to a crash when a chart was opened in parallel.

  • While going online to a Simocode Pro V PN a crash could happen when the device was still in start-up phase.

  • Repeated license check had impact on performance. This has been improved now. 

Installation instructions:

  • Updates are cumulative and contain all previous updates.

  • The update can only be installed if SIMOCODE ES V13 SP1 (TIA Portal) is already installed (109347377).

  • After each installation of SIMOCODE ES V13 SP1 (TIA Portal), the latest update needs to be installed.


Download:

 Registrierung notwendig  SIMOCODE_ES_V13_SP1_Upd3.exe (241,3 MB)



Overview of earlier versions:

Status December 2015: Update 2

This update is valid for the following product:

  • SIMOCODE ES V13 SP1 (TIA Portal)

Improvements compared to earlier versions:

Licensing

In addition to already existing license keys, also Master License Keys (MLK) for SIMOCODE ES V13 (in preparation) are supported now.

Handling of  IP addresses

The behavior of the input fields for IP addresses and station names have been improved.

An address entered in the "Properties" dialog will be automatically entered in the Parameterization Editor and vice versa. The editors now always display the same data.

The PROFINET station name corresponds by default to the device name defined in the project. If desired, the automatic generation of the station name can be turned off in the properties menu. An adjustment in the Parameter Editor is no longer necessary.

 

In conjunction with PROFINET devices Note the following:

Devices connected to an enterprise network or directly to the internet must be appropriately protected against unauthorized access, e.g. by use of firewalls and network segmentation. For more information about industrial security, please visit http://www.siemens.com/industrialsecurity

 

Bug-fixing:

The migration possibilities of SIMOCODE ES 2007 projects with SIMOCODE Pro V PN devices have been expanded.

After an upload from a device with older parameterization it will no longer cause problem with the parameters for motor protection and control device.

The wizard for setting up new equipment now offers templates for SIMOCODE ProV Modbus. The standard digital outputs module for safety applications are now completely taken over.

 

Installation instructions:

  • Updates are cumulative and contain all previous updates.
  • The update can only be installed if SIMOCODE ES V13 SP1 (TIA Portal) is already installed (109347377).
  • After each installation of SIMOCODE ES V13 SP1 (TIA Portal), the latest update needs to be installed.

 

Download:

 Registrierung notwendig  SIMOCODE_ES_V13_SP1_Upd2.exe (242,3 MB)

 

 

Status August 2015: Update 1

This update is valid for the following product:

  • SIMOCODE ES V13 SP1 (TIA Portal)

Improvements compared to earlier versions:

  • Stability when working with SIMOCODE pro V Modbus RTU has been improved.
  • As a pre-condition for working with the SIMOCODE pro V Modbus RTU basic unit, the Hardware Support Package “HSP0115 SIMOCODE pro V Modbus RTU“ needs to be installed (109476672).

Installation instructions:

  • Updates are cumulative and contain all previous updates.
  • The update can only be installed if SIMOCODE ES V13 SP1 (TIA Portal) is already installed.
  • After each installation of SIMOCODE ES V13 SP1 (TIA Portal), the latest update needs to be installed.

Download

 Download unterliegt Exportcontrolle  SIMOCODE_ES_V13_SP1_Upd1.exe (215,9 MB)

Note: The software is subject to export restrictions. The download is only available to registered users

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.