×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109479133, Entry date: 08/17/2015
(1)
Rate

Short circuit test in accordance with the standard IEC 61439-1 for 3VA molded case circuit breaker

  • Entry
  • Associated product(s)

The 3VA molded case circuit breaker limit the short-circuit current and energy. In case for the forward current of the applied circuit breaker is smaller than 17 kA short-circuit tests of the assemblies are not needed.

The tables show the limits of different 3VA molded case circuit breakers.

 


  Short_circuit_values_3VA.pdf (109,8 KB)

 

 

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.