×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109479441, Entry date: 03/16/2016
(0)
Rate

Record operator actions in WinCC Professional with the WinCC WebNavigator

  • Entry
  • Associated product(s)
In the pharmaceutical industry, the food and beverage sector or in other industries, documentation of operator actions in terms of tracking and tracing is becoming increasingly important.

Electronic documentation of operator actions ensures that all relevant operator actions during the production process are stored and, where necessary, acknowledged by the operator by an electronic signature and a comment.
The task is to allow full tracking and tracing, indicating who operated what when where. At the same time, it must be ensured that the logged operator actions are tamper-proof and that they can be read at any time. Operator actions must be recorded irrespective of whether they are performed over the Internet or on site using a web client or terminal client.

Solution
Using examples, this application shows the use of the SIMATIC WinCC WebNavigator option in conjunction with SIMATIC Logon to document process interventions with user-defined operator messages. It differentiates between the VBS and C script languages that are available in SIMATIC WinCC Professional. The application also explains the difference between logging operations on a standard operator station and operations that are performed using a SIMATIC WinCC WebNavigator Client.



Documentation and example project
  Documentation (3,3 MB)
 Registrierung notwendig  Project for TIA Portal V15.1 (3,4 MB)

Further Information
Application Example - Record operator actions via the WinCC WebNavigator
Application Example - Remote Control of Operator Panels in Applications Requiring Validation
Application Example - Operator panel remote control in the pharmaceutical environment (TIA Portal)


Last Changes  
Update TIA Portal V15.1

Additional Keywords
Audit, remote control, terminal, pharma, GMP, life science, validation, FDA 21 CFR Part 11

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.