×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109479569, Entry date: 06/14/2016
(8)
Rate

WinCC/PerformanceMonitor Plant Configurations and Installation

  • Entry
  • Associated product(s)
With the WinCC/PerformanceMonitor plant-specific figures for individual aggregates, machines or entire production lines can be calculated and analyzed in machine or line-oriented production plants.

This can be the following:

  • OEE - Overall Equipment Efficiency,

  • MTBF - Mean Time Between Failures

  • MRT - Mean Repair Time

  • and other Key Performance Indicators (KPIs)

In the process, the plant-specific production equipment can be individually defined.



This document describes the installation of the WinCC/Performance Monitor, different plant configurations and furthermore the use of the SIMATIC Information Server is described with examples in conjunction with the
WinCC/Performance Monitor.

Documentation
Registration required WinCC/Performance Monitor Plant Configuration and Installation (2.3 MB)

Further Information