×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109479635, Entry date: 04/12/2018
(4)
Rate

Which SCALANCE W products with Standard 802.11n replace the old devices without Standard 802.11n?

  • Entry
  • Associated product(s)
With the implementation of the new WLAN Standard 802.11n in the SCALANCE W products, the modules have been completely innovated and the old devices discontinued. The new devices cannot be used as replacements for the old devices.

Therefore you cannot slot the C plug of a defective old device in a new device. The new device has to be reconfigured to set it correctly. The new device in the WLAN is then compatible with the old devices.

Since the new devices are not replacements, there is no successor product listed for the old devices. This entry helps with the use of an old device.

Migration
Table 01 shows the recommended use for each article number of the old devices. For some old devices there are two new WLAN devices lists as replacements, because the number or type of connections has changed, for example. To simplify your choice, the connections are also listed separately.
In the old devices the iFeatures were included in certain products. In the new devices the iFeatures have to be enabled with the additional key plug. This is only necessary if you want to use the iFeatures.
 

Old deviceRecommended replacement
designationArticle numberConnection Antenna / LANDegree of protectionDesignationArticle numberConnection Antenna / LANDegree of protection
SCALANCE
W741-1
6GK5744-1AA30-2AA02xR-SMA/ 1xRJ45IP30SCALANCE
W721-1 RJ45
6GK5721-1FC00-0AA01xR-SMA/ 1xRJ45IP20
SCALANCE
W734-1 RJ45
6GK5734-1FX00-0AA02xR-SMA/ 2xRJ45 IP30
SCALANCE
W744-1 PRO
6GK5744-1AA60-2AA02xR-SMA/ 1xM12 IP65SCALANCE W734-1 RJ456GK5734-1FX00-0AA02xR-SMA/ 2XRJ45IP30
SCALANCE
W748-1 M12
6GK5748-1GD00-0AA03xN-Connect/ 1xM12IP65
SCALANCE W738-1 M126GK5738-1GY00-0AA02xN-Connect/ 2xM12IP65
SCALANCE
W746-1
6GK5746-1AA30-4AA02xR-SMA/ 1xRJ45 IP30SCALANCE
W721-1 RJ45
6GK5721-1FC00-0AA01xR-SMA/ 1xRJ45IP20
SCALANCE
W734-1 RJ45
6GK5734-1FX00-0AA02xR-SMA/ 2xRJ45IP30
SCALANCE
W746-1 PRO
6GK5746-1AA60-4AA02xR-SMA/ 1xM12IP65SCALANCE W734-1 RJ456GK5734-1FX00-0AA02xR-SMA/ 2XRJ45IP30
SCALANCE
W748-1 M12
6GK5748-1GD00-0AA03xN-Connect/ 1xM12IP65
SCALANCE W738-1 M126GK5738-1GY00-0AA02xN-Connect/ 2xM12IP65
SCALANCE
W747-13)
6GK5747-1AA30-6AA02xR-SMA/ 1xRJ45 IP30SCALANCE
W722-1 RJ45
6GK5722-1FC00-0AA01xR-SMA/ 1xRJ45IP20
SCALANCE W734-1 RJ456GK5734-1FX00-0AA01)2xR-SMA/ 2xRJ45IP30
SCALANCE W747-1RR3)6GK5747-1AA60-6AA02xR-SMA / 1xM12IP65SCALANCE
W748-1 M12
6GK5748-1GD00-0AA01)3xN-Connect/ 1xM12IP65
SCALANCE W734-1 RJ456GK5734-1FX00-0AA01)2xR-SMA/ 2XRJ45IP30
SCALANCE
W784-1
6GK5784-1AA30-2AA02xR-SMA / 1xRJ45 IP30SCALANCE W761-1 RJ45

6GK5761-1FC00-0AA0

1xR-SMA/ 1xRJ45IP20
SCALANCE
W774-1 RJ45

6GK5774-1FX00-0AA0

2xR-SMA/ 2xRJ45IP30
SCALANCE
W784-1 RR
6GK5784-1AA30-6AA02xR-SMA / 1xRJ45 IP30SCALANCE
W774-1 RJ45

6GK5774-1FX00-0AA0

2xR-SMA/ 2xRJ45 IP30
SCALANCE W786-1 PRO6GK5786-1AA60-2AA02xR-SMA / 1xRJ45 IP65SCALANCE W786-1 RJ456GK5786-1FC00-0AA03xR-SMA/ 1xRJ45IP65
SCALANCE W786-1 PRO6GK5786-1AB60-2AA02xinternal / 1xBFOC IP65SCALANCE WW786-2 SFP6GK5786-2FE00-0AA06xR-SMA/ 2xSFPIP65
SCALANCE W786-1 PRO6GK5786-1BA60-2AA02xinternal / 1xRJ45IP65SCALANCE W786-2IA 2RJ456GK5786-2HC00-0AA06xinternal / 1xRJ45IP65
SCALANCE W786-2PRO6GK5786-2AA60-2AA04xR-SMA / 1xRJ45 IP65SCALANCE W786-2 RJ456GK5786-2FC00-0AA06xR-SMA/ 1xRJ45IP65
SCALANCE W786-2 RR3)6GK5786-2AA60-6AA04xR-SMA / 1xRJ45 IP65SCALANCE W786-2 RJ456GK5786-2FC00-0AA02)6xR-SMA/ 1xRJ45IP65
SCALANCE W786-2PRO6GK5786-2AB60-2AA04xR-SMA / 1xBFOC IP65SCALANCE WW786-2 SFP6GK5786-2FE00-0AA06xR-SMA/ 2xSFPIP65
SCALANCE W786-2PRO6GK5786-2BA60-2AA04xinternal / 1xRJ45 IP65SCALANCE W786-2IA 2RJ456GK5786-2HC00-0AA06xinternal / 1xRJ45IP65
SCALANCE W786-2 RR3)6GK5786-2BA60-6AA04xinternal / 1xRJ45IP65SCALANCE W786-2IA 2RJ456GK5786-2HC00-0AA02)6xinternal / 1xRJ45IP65
SCALANCE W786-3PRO6GK5786-3AA60-2AA06xR-SMA / 1xRJ45 IP65SCALANCE W786-2 RJ456GK5786-2FC00-0AA06xR-SMA/ 1xRJ45IP65
SCALANCE W786-3PRO6GK5786-3AB60-2AA06xR-SMA / 1xSTIP65SCALANCE WW786-2 SFP6GK5786-2FE00-0AA06xR-SMA/ 2xSFPIP65
SCALANCE W788-1 PRO6GK5788-1AA60-2AA02xR-SMA / 1xRJ45IP65SCALANCE
W774-1 RJ45

6GK5774-1FX00-0AA0

2xR-SMA/ 2xRJ45IP30
SCALANCE W788-1 M126GK5788-1GD00-0AA03xN-Connect/ 1xM12 IP65
SCALANCE W778-1 M126GK5778-1GY00-0AA02xN-Connect/ 2xM12 IP65
SCALANCE W778-1 M12 EEC6GK5778-1GY00-0TA02xN-Connect/ 2xM12IP65
SCALANCE W788-1 RR3)6GK5788-1AA60-6AA02xR-SMA / 1xRJ45IP65SCALANCE
W774-1 RJ45
6GK5734-1FX00-0AA02)2xR-SMA/ 2xRJ45IP30
SCALANCE W788-1 M126GK5788-1GD00-0AA02)3xN-Connect/ 1xM12IP65 
SCALANCE W778-1 M126GK5778-1GY00-0AA02xN-Connect/ 2xM12 IP65
SCALANCE W778-1 M12 EEC6GK5778-1GY00-0TA02xN-Connect/ 2xM12IP65
SCALANCE W788-2 PRO6GK5788-2AA60-2AA04xR-SMA / 1xRJ45IP65SCALANCE W788-1 M126GK5788-2GD00-0AA06xN-Connect/ 1xM12IP65
SCALANCE W788-2 RR3)6GK5788-2AA60-6AA04xR-SMA / 1xRJ45IP65SCALANCE W788-1 M126GK5788-2GD00-0AA02)6xN-Connect/ 1xM12IP65

Table 01

1) iFeatures with key plug 6GK5907-4PA00
2) iFeatures with key plug 6GK5907-8PA00
3) iFeatures integrated in device

Devices for the US market
The devices for the US market differ from those for the rest of the world only in the last digits of the article number. They end in "...-0AB0" instead of "...-0AA0". Therefore Table 01 is also valid for the US market.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.