×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109479728, Entry date: 03/01/2019
(118)
Rate

Library of general functions (LGF) for SIMATIC STEP 7 (TIA Portal) and SIMATIC S7-1200 / S7-1500

  • Entry
  • Associated product(s)
The library "LGF (Library of general functions)" contains additional functions for STEP 7 (TIA Portal).

STEP 7 in TIA Portal already has an extensive number of instructions for PLC programming (mathematical functions, times, counters, etc.). In addition, there are other useful basic functions that are often required in automation projects.
 


Such general-purpose functions are provided as "Library of General Functions". This library can be used unrestricted and contains features such as FIFO, search function, matrix calculations, astro timer, ....

These functions

  • are immediately usable by parameterization
  • can be used universally
  • are not protected and therefore customizable
  • are best documented including interface description

All blocks in the library can be universally used with the following controller:

  • SIMATIC S7-1200 and S7-1200F product family (from firmware V4.2)
  • SIMATIC S7-1500 and S7-1500F product family (from firmware V2.0)
  • Simulation with SIMATIC S7-PLCSIM (as of V14)

Download for TIA Portal V14 SP1
  Documentation LGF V4.0.2 (4,0 MB)
 Registrierung notwendig  TIA Portal V14 SP1 Library LGF V4.0.2 (1,6 MB)

Download for TIA Portal V15.1 Update 1
  Documentation LGF V4.0.3 (3,7 MB)
 Registrierung notwendig  TIA Portal V15.1 Library LGF V4.0.3 (1,7 MB)


Note for FB LGF_TimerSwitch
Concerns only users, who use the FB LGF_TimerSwitch from the library V 4.0.0 for TIA portal V14 SP1 or the library V 4.0.1 for TIA portal V15 in a project.
  Note for FB LGF_TimerSwitch (560,7 KB)


Further Information
The LGF was created with the programming styleguide. 
Library with program examples for TIA Portal instructions
Library with PLC data types (LPD) for STEP 7 (TIA Portal) and S7-1200 / S7-1500

Last change
LGF V4.0.3
See chapter history in the documentation

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.