×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109479783, Entry date: 10/01/2015
(2)
Rate

Announcement of product phase-out of the external prommer "SIMATIC USB Prommer"

  • Entry
  • Associated product(s)
The external prommer "SIMATIC USB Prommer" is declared a phase-out product with effect from 1 October 2015.

The declared phase-out with effect from 1 October 2015 affects the following order number:


 

  order number
 6ES7792-0AA00-0XA0 SIMATIC USB Prommer

 


There are no plans for a successor of the SIMATIC USB Prommer.

The external prommer can still be obtained as a phase-out product using the same order process as before.


 

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.