×
Siemens Industry Online Support
Siemens AG
文档类型 应用与工具 文档编号 109479885, 文档发布日期 2018年10月8日
(1)
评估

SIMATIC RF650M data synchronization

  • 文档
  • 涉及产品
The mobile SIMATIC RF650M UHF RFID reader was designed for flexible use under difficult conditions. This application example shows you how you can transfer read transponder data via a WLAN interface directly to a PC or S7 controller.

The comprehensive "RF650M" software supplied with the SIMATIC RF650M offers all functions required for reading and handling UHF transponders. There is only one function missing on the mobile handheld reader for the automatic transfer of read transponder data to a remote PC or S7 controller.

Solution

In this application example the WLAN interface of the SIMATIC RF650M is used to send transponder data to a remote PC or PLC. For this purpose, simple applications and blocks have been created - one application for the mobile handheld reader and for the PC and S7 blocks for S7 controllers. The applications/blocks establish a TCP connection to each other and exchange the transponder data through it.

The transponder data is read out and transmitted via the mobile application. The PC application or S7 blocks only receives the transponder data and displays it to the user.
 

安全性信息
为了保护技术基础设施、系统、机器和网络免受网络威胁,有必要实施并持续维护一个全面、最先进的IT安全方案。西门子的产品和解决方案构成了这一方案的一个要素。有关网络安全的更多信息,请访问
https://www.siemens.com/cybersecurity#Ouraspiration.