×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 109480073, Entry date: 10/15/2015
(1)
Rate

SinuTrain for SINUMERIK Operate 4.5 Ed.2 - MCT: Information on the creation of a machine adjustment

  • Entry
  • Associated product(s)
A correctly created archive from the controller shall be converted into a SinuTrain machine adjustment using the machine configuration tool (MCT) V4.5 Ed.2. After selecting the archive and entering the requested data, the adjustment process is, however, aborted.

Question
How can I convert the archive without errors?

Answer
On account of the complexity of the real machine, a complete archive (created using the shortcut CTRL+ALT+S) may exceed an internal size limitation. In most cases, files in the HMI share of the archive are the reason for the enormous file size.

Before you can create a machine adjustment, you must reduce the archive. However, it would be easier to use a mere NC archive (without HMI, PLC, DRV share). If HMI screens are required, these can be integrated subsequently in accordance with the following FAQ: 85065340

Note
Changes to the HMI path are performed on the user’s own risk, support is not provided by SIEMENS.

Supplementary search terms
sinutrainforoperate

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.