×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109481531, Entry date: 05/31/2016
(8)
Rate

SINAMICS G110M AS-Interface control function blocks

  • Entry
  • Associated product(s)
The SINAMICS G110M implements AS-Interface communication with the control unit CU240M AS-i. The drive can therefore be controlled with AS-i-masters. This application offers control function blocks for Step 7 V5.5 and TIA V13 Sp1 for cyclic and acyclic communication.

Task
The digital and the cyclic control and status signals of a SINAMICS G110M AS-i-Slave should be cyclically written or read by an AS-I master. Further, the acyclic parameter access to read or write parameters or to perform basic commissioning of a SINAMICS G110M via an AS-i master should also be possible. At the one hand varying configuration of SINAMICS G110M AS-i slaves must be possible and on the other various AS-i master should be applicable.

 

Solution
The application is based on proven AS-I control blocks used in conveyor applications for the motor starter M200D and the drive SINAMICS G110D. The common AS-i masters can be used to perform the cyclic and acyclic data exchange with the SINAMICS G110M easily.

 


 

Downloads

STEP7 V5.5
 Manual 12/2015 (741,6 KB)
 Registrierung notwendig G110M V1.0 (843,6 KB)

TIA Portal V13 Sp1
 Manual 05/2016 (970,4 KB)
 Registrierung notwendig G110M AS-i V1.1 (10,5 MB)
 Registrierung notwendig LASiCom function block library (1,5 MB)

Additional Search Terms 
motioncontrol_apc_applications, Fördertechnik, conveyor systems, AS-Interface, Ansteuerbausteine, control blocks

 

 

Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.