×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109481769, Entry date: 12/21/2015
(0)
Rate

Sales and Delivery Release of Firmware V2.6 for TIM 3V-IE, TIM 3V-IE Advanced and TIM 4R-IE

  • Entry
  • Associated product(s)
The new Firmware V2.6 for SINAUT communication modules TIM 3V-IE, TIM 3V-IE Advanced and TIM 4R-IE is released and available for download effective immediately. The modules are planned for release in the middle of January 2016 with the new V2.6 firmware.


1. Product description


Firmware V2.6 contains the following additional functions and changes:

  • Introduction of the "PathStatus" system object for displaying the path status from the perspective of the local TIM to a partner.

  • TIM 4R-IE only: The reception of time-of-day synchronization via the S7 multicast service is not enabled when a local ST7cc/SCADA is configured. This is intended to avoid receiving synchronization from two different time sources.

  • Correction of SSA-763427: Vulnerability in Communication Processor (CP) modules SIMATIC CP 343-1, TIM 3V-IE, TIM 4R-IE, and CP 443-1: http://www.siemens.com/cert/en/cert-security-advisories.htm.


Performing an upgrade using a free firmware update is generally expedient and is recommended.

Note: The firmware may be subject to export restrictions; download is only possible for registered users.


2. Ordering data

Product name

Order number

TIM3V-IE

6NH7800-3BA00

TIM 3V-IE Advanced

6NH7800-3CA00

TIM4R-IE

6NH7800-4BA00


3. Miscellaneous


TIM V2.6 is backward compatible to the previous version. SINAUT Engineering Software as of version 5.5 + SP1 should be employed to use the new functions

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.