×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109481850, Entry date: 01/04/2016
(0)
Rate

Sales release for SIMOTICS S-1FG1 (stage 2)

  • Entry
  • Associated product(s)
In the second stage the new SIMOTICS S-1FG1 servo geared motors in shaft heights 80 and 100 as well as gearbox sizes 109, 129 and 149 have now been released for sale.

Basic information on the sales release

This sales release is coupled to a limited delivery release. This means that the servo geared motors can initially only be offered to specific customers. This restriction does not apply to the SIMOTICS S-1FG1 servo geared motors with shaft heights of 36, 48 and 63.

Product description

The second stage of the SIMOTICS S-1FG1 sales release includes the following gearbox types and sizes:

  • Helical geared motors (two- and three-stage): Z109, D109, Z129, D129
  • Parallel shaft geared motors (two- and three-stage): FZ109, FD109, FZ129, FD129
  • Bevel geared motors (two- and three-stage): K129, K149

See the graphic for the available gearbox sizes:


The following options have also been released:

  • Spring-loaded brakes with increased energy capability for shaft heights 80-100 with optional manual brake release und wear check
  • Version for increased chemical resistance
  • Inclined mounting positions

Documentation

  • The D41 Catalog has been supplemented with the relevant shaft heights and gearbox sizes. The Catalog will initially be available as a pdf file for downloading in theInformation and Download Center.
  • The printed version of the Catalog is scheduled for spring 2016

Additional information

SIMOTICS S-1FG1

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.