×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109482134, Entry date: 01/21/2016
(0)
Rate

MASTERDRIVES vector control (CU2) – Z option V04

  • Entry
  • Associated product(s)
The significance of the Z option V04 for MASTERDRIVES vector control (CU2) is explained.

Question:
What is the significance of the Z option V04 for MASTERDRIVES vector control (CU2)?

Answer:
The Z option V04 for Masterdrives VC (CU2) means that the control module CU2 was shipped with firmware version V1.34. At this point in time V1.34, was not a generally released version. V1.34 was necessary if customers wished to use the Z option K80 (Safe Stop).

Alternative, for a defective CU2:
Replacement of the control module MASTERDRIVES vector control (CU2) by MASTERDRIVES vector control (CUVC).
Also refer to FAQ "MASTERDRIVES Vector Control CUVC as successor for MASTERDRIVES Vector Control CU2", Entry ID 22642090.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit