×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109482396, Entry date: 02/22/2019
(20)
Rate

Libraries with PLC data types (LPD) for STEP 7 (TIA Portal) and SIMATIC S7-1200 / S7-1500

  • Entry
  • Associated product(s)
The library “LPD (Library of PLC Data types)" contains PLC data types which describe the data structure of the address spaces and the data records of peripheral / technology modules and PROFIdrive drives.

In the respective manuals of the peripheral and technology modules, the address spaces (control and feedback interface) and the individual parameter data records are described. The library LPD (library of PLC data types) provides these address spaces and parameter data records in the form of individual PLC data types.

The following figure shows the structure of the library and the supported modules.




With the PLC data types for the
  • address spaces, you can create PLC tags and with them symbolically and structurally access the input and output area in the user program.
  • With parameter data records, you can create data records to parameterize modules which can then be transferred to the modules via the WRREC instruction.

Documentation and project example
  Documentation (1,7 MB)
 Registrierung notwendig  LPD (Library of PLC Datatypes) for TIA Portal V15.1 (1,2 MB)

The library LPD has been created with the programming style. 81318674

Last change
Expansions:

  • PROFIdrive telegrams
  • Analog modules for SIMATIC ET 200SP / ET 200MP
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.