×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109482434, Entry date: 02/04/2016
(28)
Rate

SIMATIC WinCC SmartClient.exe remote maintenance for SIMATIC HMI

  • Entry
  • Associated product(s)
To use SmartClient.exe without the installation of the engineering- or runtime systems e.g. for service purposes, SmartClient.exe can be downloaded for free.

The access to a HMI configured as a smart server is possible over the following ways

  • SIMATIC WinCC SmartClient App for Android and iOS ( www.siemens.de/simatic2go )
  • WebBrowser via the SmartClient-JavaApplet (will be downloaded automatically from smart server)
  • Windows PC with SmartClient.exe

To use SmartClient.exe without the installation of the engineering- or runtime systems e.g. for service purposes, SmartClient.exe can be downloaded for free. In addition, SmartClient.exe can also be installed via the product DVD of WinCC flexible or WinCC (TIA Portal).


Download SmartClient.exe:

Due to the statutory regulations for export control the SmartClient.exe is offered with registration only. According to the registration the SmartClient.exe can be downloaded free of charge.

 Download unterliegt Exportcontrolle  SmartClient_V17.exe (596,0 KB)(SHA-256)


Copy from a PC with installed WinCC Runtime Advanced or WinCC flexible Runtime

If WinCC flexible Runtime or WinCC runtime advanced is installed on the smart client PC, the smart client application was installed automatically in the following folder and can be copied from there.

WinCC flexible Engineering DVD (Micro / Compact / Standard / Advanced):

  • ...\Program files\Siemens\WinCC flexible\WinCC flexible RT\SmartClient.exe

WinCC (TIA Portal) Engineering DVD (Basic / Comfort / Advanced / Professional):

  • ...\Program files\Siemens\Automation\WinCC RT Advanced\SmartClient.exe


Copy from product DVD

The SmartClient.exe can be copied from the following folders of respective WinCC product DVDs:

WinCC flexible Engineering DVD (Micro / Compact / Standard / Advanced):

  • ...\Support\SmartClient\SmartClient.exe

WinCC (TIA Portal) Engineering DVD (Basic / Comfort / Advanced / Professional):

  • ...\Support\SmartClient\SmartClient.exe
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.