×
Siemens Industry Online Support
Siemens AG
Entry type: Application example, Entry ID: 109482515, Entry date: 08/02/2018
(25)
Rate

Demo project for SIMATIC WinCC V7.4 SP1

  • Entry
  • Associated product(s)
This page contains the current SIMATIC WinCC V7.4 SP1 demo projects (example configuration) for download. The “use-case oriented” projects provide a guided tour through the plant with different user names.

Description:
The demo project is configured in German and English.
The UI language can be set individually in the development environment of SIMATIC WinCC V7.4 SP1.
The configured national languages are also available in Runtime.

Demo project
 Registrierung notwendig  WinCC V7.4 SP1 demo project (336,1 MB)

Description WinCC project (videos)
start WinCC project


operate WinCC project


SIMATIC WinCC SCADA in Online Support
The overview page displays all information on the topic of WinCC at a glance.
You can find the page in entry ID 93906404.

Demo projects for SIMATIC WinCC V7.3
Demo projects for the previous WinCC V7.3 version can be found in the following entry ID: 76879225.

Demo projects for WinCC Runtime Professional V13
Demo projects for WinCC Runtime Professional including Multitouch gestures can be found in the following entry ID: 109478972.

SIMATIC WinCC V7.4 Trial Software, Europa and Asia
The software required for using the demo projects can also be obtained as trial software (for 30 days) from the sales partner responsible.
Siemens Contact Person

Trial DVD WinCC V7.4
Article No. 6ZB5370-1DN70-2FA8

Further information on WinCC V7.4 is available in the following entry ID 109483726

WinCC V7.4 supports the following Microsoft operating systems
For WinCC single-user projects and client projects

Support of 32-bit operating systems

  • Windows 7 SP1 Professional, Enterprise and Ultimate for WinCC Single-user / Client System

  • Windows 8.1 Professional, Enterprise for WinCC Single-user / Client System

Support of 64-bit operating systems

  • Windows 10 Professional, Enterprise for WinCC Server/ Single-user/ Client System
    Further information regarding Windows 10 see entry ID 109482899
  • Windows 7 SP1 Professional, Enterprise and Ultimate for WinCC Server / Single-user / Client System
  • Windows 8.1 Professional, Enterprise for WinCC Server / Single-user / Client System
  • Windows 2008 Server R2 SP1 Standard, Enterprise for WinCC Server / Single-user system
  • Windows 2012 Server R2 Standard, Enterprise for WinCC Server / Single-user System
Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.