×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109482560, Entry date: 07/11/2016
(0)
Rate

How do you configure communication via Modbus/TCP with WinAC RTX (F) in TIA Portal V13 SP1?

  • Entry
  • Associated product(s)
This FAQ offers step-by-step instructions on how to use the SIMATIC Modbus/TCP software with a WinAC RTX (F) software PLC in TIA Portal V13 SP1.

SIMATIC WinAC RTX (F)
SIMATIC WinAC RTX (F) is the SIMATIC software controller for PC-based automation solutions and allows real-time deterministic control on the PC.


SIEMENS Modbus/TCP Software
MODBUS is a worldwide communication protocol which is open to all users and is used by many manufacturers. On this basis, MODBUS/TCP has been developed for the use in modern networks. In today’s industry, this protocol has become a de facto standard which has been introduced in the Internet Engineering Task Force (IETF) – an organization responsible for Internet standardization.

The SIMATIC Modbus/TCP software packages offer ready-to-use blocks for simple and quick implementation of a MODBUS communication in SIMATIC controllers.

 


Figure 1


Download
 Documentation (1,0 MB)


Related information
Find more information on the SIMATIC Modbus/TCP software at http://www.siemens.com/s7modbus
Find another application example on Modbus TCP communication at 75312612

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.