Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 109482560, Entry date: 07/11/2016

How do you configure communication via Modbus/TCP with WinAC RTX (F) in TIA Portal V13 SP1?

  • Entry
  • Associated product(s)
This FAQ offers step-by-step instructions on how to use the SIMATIC Modbus/TCP software with a WinAC RTX (F) software PLC in TIA Portal V13 SP1.

SIMATIC WinAC RTX (F) is the SIMATIC software controller for PC-based automation solutions and allows real-time deterministic control on the PC.

SIEMENS Modbus/TCP Software
MODBUS is a worldwide communication protocol which is open to all users and is used by many manufacturers. On this basis, MODBUS/TCP has been developed for the use in modern networks. In today’s industry, this protocol has become a de facto standard which has been introduced in the Internet Engineering Task Force (IETF) – an organization responsible for Internet standardization.

The SIMATIC Modbus/TCP software packages offer ready-to-use blocks for simple and quick implementation of a MODBUS communication in SIMATIC controllers.


Figure 1

 Documentation (1,0 MB)

Related information
Find more information on the SIMATIC Modbus/TCP software at http://www.siemens.com/s7modbus
Find another application example on Modbus TCP communication at 75312612

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit