×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109482659, Entry date: 01/30/2019
(10)
Rate

SINAMICS Firmware Version 4.7 SP6 HF5 for SINAMICS products G120 (CU230P-2, CU240B/E-2, CU250S-2), G120C, G120D (CU240D-2, CU250D-2), G110M and SIMATIC ET200pro FC-2

  • Entry
  • Associated product(s)
In this article you will find the download as well as the ordering information for SINAMICS G120 multicard with version V4.7 SP6 HF5.

Important Note

The SINAMICS G120 Firmware Version 4.7 SP6 has achieved the milestone "Phase-out announcement" on 01.10.2018. With this background, we recommend using the latest SINAMICS G firmware. The milestone P.M410 "Product Cancellation" for V4.7 SP6 is planned for 01.10.2019.


For the latest firmware version please refer to the article 67364620.

 

Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the READ_OSS.HTM file.


Special information for resellers

The information and the license terms in the READ_OSS.HTM file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.


Availability of Source Code

Certain license conditions of third-party software components used in this product may require Siemens to provide you with the source code and additional information for such components. In most cases, Siemens provides this information on or with the device. In case Siemens is technically unable to do so, you may request a copy of of this OSS source code against payment of shipping and handling charges. Please send your request to the address provided at the end of this section.


Siemens AG 

Digital Factory

Customer Services DF&PD

DF CS SD CCC TS

Gleiwitzer Str. 555

90475 Nuernberg, Deutschland

Internet: http://www.siemens.com/automation/support-request

Tel.: +49 911 895 7222


  READ_OSS.HTM (1,1 MB)

 

Current list of secondary conditions of the SINAMICS G120 for firmware V4.7 SP6 HF5

  SINAMICS_G120_V476_General_Conditions.PDF (31,5 KB) 

 

Provision of the SINAMICS G120 multicard V4.7 SP6 HF5

The content of the SINAMICS G120 multicard described above can be downloaded here:


Note:
From version V4.7 HF3, the runtime SINAMICS G120 firmware is not subject to any export restrictions as the output frequency has been limited to 550 Hz. It is not subject to the Iran embargo, and is not listed in the EC Dual Use regulation. (AL = N). It does not involve a US product (ECCN = N). Alternatively, the SINAMICS G120 multicard V4.7 SP6 HF5 (SD card) can be ordered using the following order number 6SL3054-7TD00-2BA0.


Instructions for updating the firmware of the SINAMICS G120:

When upgrading, please refer to the instructions, Chapter "Firmware update" in the operating instructions of the particular Control Unit.

For example, you can find the firmware upgrade/downgrade instructions for CU240B-2 and CU240E-2 here:

  FW_Upgrade_Downgrade_en.pdf (467,7 KB)


Note:

The zip file on the SD memory card must be unzipped to the root directory. A SD memory card with at least 256 MB must be used. Memory cards larger than 2 GB are not supported. The SD-CARD 512 MB EMPTY can be ordered by specifying the following order number 6SL3054-4AG00-2AA0.


Functional restrictions which have been corrected for the SINAMICS G120 firmware V4.7 SP6 HF5

 Registrierung notwendig  Corrected_Functional_Restrictions_G120_V4.7_SP6_HF5.pdf (21,9 KB) 

 


List of faults and alarms

List of faults and alarms for CU230P-2


The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the G120P in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, support can no longer be guaranteed for the G120P product.

  alarmlist_g120_cu230p_v04707900_chs.xml (380,7 KB)

  alarmlist_g120_cu230p_v04707900_eng.xml (411,6 KB)

  alarmlist_g120_cu230p_v04707900_esp.xml (433,0 KB)

  alarmlist_g120_cu230p_v04707900_fra.xml (444,0 KB)

  alarmlist_g120_cu230p_v04707900_ita.xml (439,3 KB)

  alarmlist_g120_cu230p_v04707900_rus.xml (546,8 KB)

  alarmlist_g120_cu230p_v04708200_deu.xml (417,1 KB)

 


List of faults and alarms for the CU240B-2 and CU240E-2

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text of the G120 in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, no additional support can be guaranteed for the G120 product.
 

  alarmlist_g120_cu240b_e_v04707900_chs.xml (620,7 KB)

  alarmlist_g120_cu240b_e_v04707900_eng.xml (671,6 KB)

  alarmlist_g120_cu240b_e_v04707900_esp.xml (705,6 KB)

  alarmlist_g120_cu240b_e_v04707900_fra.xml (725,6 KB)

  alarmlist_g120_cu240b_e_v04707900_ita.xml (712,4 KB)

  alarmlist_g120_cu240b_e_v04707900_rus.xml (892,9 KB)

  alarmlist_g120_cu240b_e_v04708200_deu.xml (680,4 KB)



List of faults and alarms for the CU240D-2 and CU250D-2

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the G120D in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, no additional support can be guaranteed for the G120D product.


  alarmlist_g120d_v04707900_chs.xml (710,3 KB)

  alarmlist_g120d_v04707900_eng.xml (769,9 KB)

  alarmlist_g120d_v04707900_esp.xml (807,1 KB)

  alarmlist_g120d_v04707900_fra.xml (829,7 KB)

  alarmlist_g120d_v04707900_ita.xml (816,0 KB)

  alarmlist_g120d_v04707900_rus.xml (1,0 MB)

  alarmlist_g120d_v04708200_deu.xml (776,5 KB)

 

Listen der Störungen und Warnungen für die CU250S-2

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the G120 in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, no additional support can be guaranteed for the G120 product.


  alarmlist_g120_cu250s_v04707900_chs.xml (1,1 MB)

  alarmlist_g120_cu250s_v04707900_eng.xml (1,2 MB)

  alarmlist_g120_cu250s_v04707900_esp.xml (1,2 MB)

  alarmlist_g120_cu250s_v04707900_fra.xml (1,3 MB)

  alarmlist_g120_cu250s_v04707900_ita.xml (1,3 MB)

  alarmlist_g120_cu250s_v04707900_rus.xml (1,6 MB)

  alarmlist_g120_cu250s_v04708200_deu.xml (1,2 MB)

 


List of faults and alarms of the G120C

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the G120C in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, no additional support can be guaranteed for the G120C product.


  alarmlist_g120c_v04707900_chs.xml (427,9 KB)

  alarmlist_g120c_v04707900_eng.xml (466,0 KB)

  alarmlist_g120c_v04707900_esp.xml (490,7 KB)

  alarmlist_g120c_v04707900_fra.xml (504,9 KB)

  alarmlist_g120c_v04707900_ita.xml (496,2 KB)

  alarmlist_g120c_v04707900_rus.xml (625,4 KB)

  alarmlist_g120c_v04708200_deu.xml (471,6 KB)

 


List of faults and alarms of the G110M

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text of the G110M in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, no additional support can be guaranteed for the G110M product.


  alarmlist_G110M_v04707900_chs.xml (532,8 KB)

  alarmlist_G110M_v04707900_eng.xml (577,2 KB)

  alarmlist_G110M_v04707900_esp.xml (607,7 KB)

  alarmlist_G110M_v04707900_fra.xml (624,7 KB)

  alarmlist_G110M_v04707900_ita.xml (614,4 KB)

  alarmlist_G110M_v04707900_rus.xml (770,0 KB)

  alarmlist_G110M_v04708200_deu.xml (584,6 KB)

 


List of faults and alarms of the ET200pro FC-2

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text of the ET200pro FC-2 in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, no additional support can be guaranteed for the ET200pro FC-2 product.


  alarmlist_et200pro_v04707900_chs.xml (552,5 KB)

  alarmlist_et200pro_v04707900_eng.xml (600,6 KB)

  alarmlist_et200pro_v04707900_esp.xml (632,3 KB)

  alarmlist_et200pro_v04707900_fra.xml (650,2 KB)

  alarmlist_et200pro_v04707900_ita.xml (639,6 KB)

  alarmlist_et200pro_v04707900_rus.xml (807,4 KB)

  alarmlist_et200pro_v04708200_deu.xml (608,6 KB)

 

GSD files for project integration into the PROFIBUS configuring tool

PROFIBUS GSD files can be downloaded in the following entries:

 

GSDML files for integrating projects into the PROFINET configuring tool

PROFINET GSDML files can be downloaded in the following entries:

 

EDS files for integrating projects into the CANopen configuring tool

The EDS files for integrating projects into the CANopen configuring tools can be downloaded from the following entry:  (see 48351511)

 

STARTER

Within the scope of firmware version V4.7 SP6 HF1, a new SINAMICS Support Package for STARTER V4.4 SP1 (see 109475420) will be provided. The SSP is available as a download via the following  artical 109477753.


With the SSP, new functions can be configured in the V4.7 SP6 HFx firmware using STARTER.

Within the scope of revising and simplifying the commissioning wizards, SINAMICS application classes "Standard Drive Control", "Dynamic Drive Control" and "Expert" have been introduced.

 

For "Standard Drive Control", after the commissioning wizards have been completed and when the drive is switched on for the first time, a shortened motor data identification routine is carried out (p1900 = 2).

 

For "Dynamic Drive Control", as default setting, a shortened motor data identification routine is selected after the drive is switched on for the first time (p1900 = 2). A rotating measurement is recommended to achieve a higher accuracy and dynamic performance of the closed-loop control.

 

Under "Expert", you will find the traditional wizard providing a multitude of setting options.


In all three application classes the type of motor data identification routine can be configured. For the motor data identification routine, you can select during commissioning whether the drive shall run up directly to the setpoint or whether another Power ON command is required.  An active motor data identification routine will be displayed in the STARTER control panel.

 

Warning

Based on V4.7 SP3: when a motor data identification (motor ID) with subsequent ramp-up to the setpoint speed (p1900 = 11 or 12; 12=standard setting with "Standard Drive Control" and "Dynamic Drive Control") was selected, the motor is, upon the first Power ON command, directly accelerated to the setpoint speed, following a short delay time caused by the motor ID (approx. 15 to 30 s). For additional information, see 109480663.


From firmware V4.7 SP6 HF1 the default settings for a motor data identification was changed in combination with the application classes "Standard Drive Control" und "Dynamic Drive Control" (p1900= 2; 2= Motor data identification (in standstill)). With this setting the motor remains in standstill after a the motor data identification was completed. To start the motor, a new start command is necessary.

 

In order to be able to use the revised commissioning wizards for G120 Control Units with PM240, PM240-2 and PM330, as well as for G120C, it is absolutely necessary to upgrade STARTER to version V4.4 SP1 inclusive the named SSP for V4.7 SP6.

 

Startdrive

Within the scope of firmware version V4.7 SP6 HF1, for Startdrive V13 SP1 (see 107657741) Support Package V4.7 SP6 is available (see 109482758).

When importing the Support Packages in an existing Startdrive V13 SP1 installation, new functions in firmware V4.7 SP6 HFx can be used with Startdrive. Included here is the revised commissioning wizard, which can be used with SINAMICS G120 Control Units in conjunction with PM240, PM240-2, PM330 Power Modules and with G120C.


Within the scope of revising and simplifying the commissioning wizards, SINAMICS application classes "Standard Drive Control", "Dynamic Drive Control" and "Expert" have been introduced.

 

For "Standard Drive Control", after the commissioning wizards have been completed and when the drive is switched on for the first time, a shortened motor data identification routine is carried out (p1900 = 2).

 

For "Dynamic Drive Control", as default setting, a shortened motor data identification routine is selected after the drive is switched on for the first time (p1900 = 2). A rotating measurement is recommended to achieve a higher accuracy and dynamic performance of the closed-loop control.

 

Under "Expert", you will find the traditional wizard providing a multitude of setting options.


In all three application classes the type of motor data identification routine can be configured. For the motor data identification routine, you can select during commissioning whether the drive shall run up directly to the setpoint or whether another Power ON command is required.  An active motor data identification routine will be displayed in the Startdrive control panel.

 

Warning

Based on V4.7 SP3: when a motor data identification (motor ID) with subsequent ramp-up to the setpoint speed (p1900 = 11 or 12; 12=standard setting with "Standard Drive Control" and "Dynamic Drive Control") was selected, the motor is, upon the first Power ON command, directly accelerated to the setpoint speed, following a short delay time caused by the motor ID (approx. 15 to 30 s). For additional information, see 109480663.


From firmware V4.7 SP6 HF1 the default settings for a motor data identification was changed in combination with the application classes "Standard Drive Control" und "Dynamic Drive Control" (p1900= 2; 2= Motor data identification (in standstill)). With this setting the motor remains in standstill after a the motor data identification was completed. To start the motor, a new start command is necessary.

  

Die Installation einer neuen Startdrive Version ist nicht notwendig.

 

IOP / BOP-2

With firmware version V4.7 SP6 HF1, the commissioning wizard has been revised. This can be used with SINAMICS G120 Control Units in conjunction with PM240, PM240-2, PM330 Power Modules and with G120C.


Within the scope of revising and simplifying the commissioning wizards, SINAMICS application classes "Standard Drive Control", "Dynamic Drive Control" and "Expert" have been introduced.

 

For "Standard Drive Control", after the commissioning wizards have been completed and when the drive is switched on for the first time, a shortened motor data identification routine is carried out (p1900 = 2).

 

For "Dynamic Drive Control", as default setting, a shortened motor data identification routine is selected after the drive is switched on for the first time (p1900 = 2). A rotating measurement is recommended to achieve a higher accuracy and dynamic performance of the closed-loop control.

 

Under "Expert", you will find the traditional wizard providing a multitude of setting options.


In all three application classes the type of motor data identification routine can be configured. For the motor data identification routine, you can select during commissioning whether the drive shall run up directly to the setpoint or whether another Power ON command is required.  An active motor data identification routine will be displayed in the Startdrive control panel.

 

Warning

Based on V4.7 SP3: when a motor data identification (motor ID) with subsequent ramp-up to the setpoint speed (p1900 = 11 or 12; 12=standard setting with "Standard Drive Control" and "Dynamic Drive Control") was selected, the motor is, upon the first Power ON command, directly accelerated to the setpoint speed, following a short delay time caused by the motor ID (approx. 15 to 30 s). For additional information, see 109480663.


From firmware V4.7 SP6 HF1 the default settings for a motor data identification was changed in combination with the application classes "Standard Drive Control" und "Dynamic Drive Control" (p1900= 2; 2= Motor data identification (in standstill)). With this setting the motor remains in standstill after a the motor data identification was completed. To start the motor, a new start command is necessary.


Expanded functionality is supported with the new IOP version from V1.6 SP2 and higher. A complete overview of the expanded functionality for IOP V1.6 SP2 can be taken from the sales and delivery release 109476464. In order to upgrade an existing IOP the entry ID also includes an IOP firmware download.


Additionally the Intelligent Operator Panel IOP-2 will be offered since June 2017. The IOP-2 can also be used in combination with SINAMICS firmware V4.7 SP6 HFx. Further details concerning IOP-2 can be found within the delivery release 109748340.


The BOP-2 operator panel (Order No.: 6SL3255-0AA00-4CA1) is automatically updated when using firmware V4.7 SP6 HF5.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.