×
Siemens Industry Online Support
Siemens AG
Type bericht: Productmededeling ID van bericht: 109482683, Datum bericht: 04/13/2016
(3)
Beoordelen

Sales release for SIMOTICS S-1FT7 and 1FK7 motors with a Pt1000 temperature sensor

  • Bericht
  • Heeft betrekking op product(en)
The 1FT7 and 1FK7 (Generation 2) series of servo motors are available with the Pt1000 temperature sensor with a changed article number with immediate effect. Initially, versions without DRIVE-CLiQ are affected. Release for the 1FK7 Generation 1 in AH20-28 is planned for May 2016.

Background

Pt1000 temperatures sensors will in the future be installed in the following SIMOTICS S servo motors without a DRIVE-CLiQ interface:

SIMOTICS S-1FT7

SIMOTICS S-1FK7 Generation 2

SIMOTICS S-1FK7 Generation 1 with shaft heights 20 and 28 (delivery release planned for May 2016)

The Pt1000 temperature sensors supersede the previously integrated KTY84-130 sensors. More information on the discontinuation of the KTY84-130 is available in the following entry 109478106

The following changes have been made:

  • Motors with a DRIVE-CLiQ interface will be fitted with Pt1000 temperature sensors at a later date. Also, from the user's viewpoint, these motors exhibit compatible temperature evaluation behavior with the Pt1000, so no further action is required.
  • Current motor series without the DRIVE-CLiQ interface with the Pt1000 temperature sensor will have a new article number because they are not compatible with the KTY84 temperature sensor.

New article numbers for SIMOTICS S-1FT7 motors without a DRIVE-CLiQ interface

For the following encoders without DRIVE-CLiQ, the 12th position of the article number must be modified accordingly.

  • Incremental encoder IC2048S/R (1FT7...-.....-.N..)
  • Absolute encoder AM2048S/R (1FT7...-.....-.M..)


1FT7 motors without DRIVE-CLiQ interface:

Old article number

with KTY84-130

New article number

with Pt1000

with recessed flange and encoder IC2048S/R

1FT7...-....0-.N..1FT7...-....5-.N..

with recessed flange and encoder AM2048S/R

1FT7...-....0-.M..1FT7...-....5-.M..

compatible flange with 1FT6/1FK7 with encoder IC2048S/R

1FT7...-....1-.N..1FT7...-....4-.N..
compatible flange with 1FT6/1FK7 with encoder AM2048S/R1FT7...-....1-.M..1FT7...-....4-.M..

For the 1FT7 with shaft height 132, there is so far no version with a KTY84-130 temperature sensor. With the introduction of Pt1000, the encoders are released without Drive CLiQ. There will be no more versions with KTY 84-130.

compatible flange with 1FT6 with encoder IC2048S/R

-1FT713.-....4-.N..
compatible flange with 1FT6 with encoder AM2048S/R-1FT713.-....4-.M..

New article numbers for

SIMOTICS S-1FK7 Generation 2 (and Generation 1 with shaft heights 20 - 28) motors without a DRIVE-CLiQ interface

For the following encoders without DRIVE-CLiQ, the 12th position of the article number must be modified accordingly.

  • Incremental encoder IC2048S/R (1FK7...-.....-.A..)
  • Absolute encoder AM2048S/R (1FK7...-.....-.E..)
  • Absolute encoder AM512S/R (1FK7...-.....-.H..)
  • Absolute encoder AM16S/R (1FK7...-.....-.J..)
  • Multi-pole resolver (1FK7...-.....-.S..)
  • 2-pole resolver (1FK7...-.....-.T..)


1FT7 Generation 2 motors without a DRIVE-CLiQ interface:

Old article number

with KTY84-130

New article number

with Pt1000

Incremental encoder IC2048S/R1FK7...-....1-.A..1FK7...-....4-.A..
Absolute encoder AM2048S/R1FK7...-....1-.E..1FK7...-....4-.E..
Absolute encoder AM512S/R1FK7...-....1-.H..1FK7...-....4-.H..
Absolute encoder AM16S/R1FK7...-....1-.J..1FK7...-....4-.J..
Multi-pole resolver1FK7...-....1-.S..1FK7...-....4-.S..
2-pole resolver1FK7...-....1-.T..1FK7...-....4-.T..

If possible, these article numbers should be used immediately for any new installations.

Compatibility with converter firmware

If converters of other manufacturers are used, compatibility with the Pt1000 temperature sensor must be checked.

If Siemens converters are used, the versions with Pt1000 will be supported by the following firmware:

Runtime:

  • SINAMICS S120 Firmware V4.8 and a hotfix for the latest Firmware V4.7
  • SINAMICS G120 Firmware V4.7 SP6
  • SINUMERIK V4.8 and hotfixes for the latest firmware versions V4.5 and V4.7
  • SIMOTION V4.5 (SINAMICS Firmware V4.8)

Commissioning tool:

  • STARTER V4.5 (SINAMICS Firmware V4.8)

The Pt1000 can be parameterized via the parameter P0601 with the value 6 for motors without DRIVE-CLiQ.

Nota's in verband met security
Ter bescherming van technische infrastructuur, systemen, machines en netwerken tegen digitale dreigingen is het noodzakelijk om een alomvattend 'IT Security' concept te implementeren (en continu te handhaven) dat overeenkomt met de huidige stand van de techniek. De producten en oplossingen van Siemens vormen slechts een klein deel van een dergelijk concept. Meer informatie over 'Cyber Security' vindt u op
https://www.siemens.com/cybersecurity#Ouraspiration.
Bericht beoordelen
geen beoordeling
Verzoeken en feedback
Wat wilt u doen?
Opmerking: de feedback heeft altijd betrekking op het actuele artikel/product. Uw bericht wordt naar de technische redacteurs van de Online Support gestuurd. We zullen binnen enkele dagen antwoorden als uw feedback dat vereist. Als we geen vragen meer hebben, zullen we geen antwoord meer sturen.