×
Siemens Industry Online Support
Siemens AG
寄稿のタイプ: 製品情報 寄稿のID: 109482717, 寄稿の日付: 02/24/2016
(0)
評価する

Improved PROFIBUS connector 6ES7972-0Bx61-0XA0

  • 寄稿
  • 製品に関係する
Effective immediately, an improved version of the existing 60-series PROFIBUS connectors with 35 degree cable outlet and displacement terminal connection is available.

Effective immediately, an improved version of the existing 60-series PROFIBUS connectors with 35 degree cable outlet and displacement terminal connection is available.

This version replaces the currently available 60-series connector with article number 6ES7 972-0B.60-0XA0. The improved connector is compatible with its predecessor in terms of functionality and spare parts. The new type with article number 6ES7 9720B.61-0XA is characterized by an improved and harmonized connection concept based on the existing PROFIBUS connectors of type 6ES7 972-0Bx42-0XA0.

In detail, the improvements in use include the fact that the lid can be kept open more easily so that it does not have to be held by hand. In addition, the walls of the basic housing are higher so that the cable strands can be held inside the connector better and do not become trapped when the lid is closed. As a result, wiring and installation of the connector becomes easier overall.


Tip:

We recommend that you use the stripping tool 6GK1 905-6AA00. There is no change for you in this respect. The stripping length for the 60-series connector should still be used.

If this tool is not available to you, please use the stripping lengths given in the instruction leaflet supplied with every connector. This leaflet can also be downloaded as a PDF file (109793857).

The dimension drawings for the PROFIBUS connectors are also available for download as PDF file (19425126). Because the dimensions of the 61-series connectors are identical to those of the 60-series connectors, please refer to the data sheet for the 60-series connector.


Order data:

Order and delivery location: LZN (Logistic Center Nuremberg)

Type

Article number

PROFIBUS connector without PG socket

6ES7 972-0BA61-0XA0

PROFIBUS connector with PG socket

6ES7 972-0BB61-0XA0

Note:

After the remaining 60-series connectors have been sold, automatic substitution with the 61-series connectors will take place.



セキュリティ情報
技術的なインフラストラクチャー、システム、機械とネットワークをサイバー脅威から守るために、現在の技術の状態に応じた全体的なITセキュリティーコンセプトを実装すること(そして持続的に維持すること)が必要です。シーメンスの製品とソリューションはそのようなコンセプトの1つの要素だけを形成します。サイバーセキュリティーについての詳細は以下をご覧ください:
https://www.siemens.com/cybersecurity#Ouraspiration.
寄稿を評価する
評価なし
リクエストとフィードバック
何をしたいですか?
注: フィードバックは常に現在のエントリ / 製品に関連しています。メッセージは、オンラインサポートで作業しているテクニカルエディタに転送されます。フィードバックに応答が必要な場合は、数日以内に返信いたします。これ以上問題がない場合、ご連絡はいたしません。
統計に対するサポート
この機能によって、希望する数に基づく検索結果のIDが出力されます (format .txt)

Generate list
URL をコピーする
このページを新しいデザインで表示する
mySupport コックピット