×
Siemens Industry Online Support
Siemens AG
Entry type: Download, Entry ID: 109483011, Entry date: 01/09/2019
(0)
Rate

Firmware SIWAREX WP251

  • Entry
  • Associated product(s)

Release V2.0.2
 Registrierung notwendig  7MH4960-6AA01_FW_V_2.0.2.zip (1,9 MB)

Changes compared to V1.0.8

  • Legal-for-trade operation as discontinuous totalizing automatic weighing instrument according OIML R-107
  • Legal-for-trade operation as automatic static check weigher according OIML R-51

An update to the newest version is recommended. The update is performed by the service software SIWATOOL V7 and explained in the following    document (586,0 KB). In addition, two SIWATOOL V7 data base files are included in the .zip-archive. These need to be copied into the SIWATOOL installation folder like described in the information.


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.