Firmware SIWAREX WP251
-
Entry
-
Associated product(s)
Release V1.0.7
WP251_FW_1_0_7.zip (436,4 KB)
Changes compared to V1.0.6
- Command acknowledgment in case of disturbed module adapted
- Modbus settings in DR12 now retained after loss of voltage
An update to the newest version is recommended. The update is performed by the service software SIWATOOL V7 and explained in the following document (586,0 KB).
Release V1.0.6


Changes compared to V1.0.4
- Fine time controller optimized
- New selection options for S7-interface
- Bugfixes
An update to the newest version is recommended. The update is performed by the service software SIWATOOL V7 and explained in the following document (586,0 KB).
In addition, two SIWATOOL V7 data base files are included in the .zip-archive. These need to be copied into the SIWATOOL installation folder like described in the information.
Release V1.0.4 / May 2017
Changes compared to V1.0.1
Support of operation on SIMATIC S7-1200 F (failsafe) controllers
Fine signal time controller for controlling the fine weight by time
Material flow calculation and monitoring by limit value
Minor fixes and optimizations
An update to the newest version is recommended. The update is performed by the service software SIWATOOL V7 and explained in the following document (586,0 KB).
In addition, two SIWATOOL V7 data base files are included in the .zip-archive. These need to be copied into the SIWATOOL installation folder like described in the information.
- German