×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109483048, Entry date: 08/09/2018
(4)
Rate

Energy monitoring and load management with PCS 7 Industry Library (Demo Project)

  • Entry
  • Associated product(s)
PCS 7 Industry Library allows the delivery of comprehensive functions for the monitoring and controlling of the energy consumption of a plant. With these functions you are able to meet an energy limit agreed with a power supply company.

Task
Certain sectors of the industry have a requirement to adhere to agreed performance limits provided by power supply companies in a defined time window. The operation of a plant without consumption monitoring may even lead to penalties. For this reason (and others) the plant operator should have an efficient load management system that monitors fuel consumption and that engages in the process if necessary.
   


   
Solution
In the example project, a local load management system is used in a pumping station together with a sludge drying plant to meet a limit agreed with a power supply company. If the projection of the power consumption exceeds the agreed limit value, the consumers are switched off or run on generators.
The documentation contains basics of load management, a description of the project structure and instructions to start and control the application.
   
Benefits
  • Time and cost savings in project planning and service
  • Increased transparency in power consumption
   
Validity  
  • SIMATIC PCS 7 V9.0 SP1 with SIMATIC PCS 7 Industry Library V9.0 Upd1
  • SIMATIC PCS 7 V8.1 with SIMATIC PCS 7 Industry Library V8.1 SP1

Documentation and demo project for PCS 7 V9.0 SP1
  Documentation (1,9 MB)
 Registrierung notwendig  Demo projekt (369,3 MB)
 Registrierung notwendig  Function block "RelEnAcq" (7,3 KB)
 Registrierung notwendig  Report template for the energy report (63,4 KB)

Documentation and demo project for PCS 7 V8.1
  Documentation (1,2 MB)
 Registrierung notwendig  Demo project (354,0 MB)

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.