×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109483152, Entry date: 11/11/2015
(6)
Rate

SSP SINAMICS G120 V4.7 SP3

  • Entry
  • Associated product(s)
SSP for updating existing STARTER resp. SCOUT installations


Current SINAMICS MICROMASTER STARTER

You can download the current STARTER here: 26233208

Description

When using this SSP, the following boundary conditions ( 1) and 2) ) must be observed:

 G120 typeCU types 

Combined with PM type (restrictions not relevant)

Combined with PM type observe restrictions 1) and  2) !

 G120

CU240B-2 or

CU240E-2 or

CU250S-2

PM230 or

PM250 or

PM260

PM240 or

PM240-2 or

PM330 or

PM340

 G120C - - X
 G120P CU230P-2

PM230 or

PM250 or

PM260

PM240 or

PM240-2 or

PM330 or

PM330L

 G120D

 CU240D-2 or

CU250D-2

PM250D -

 

SSPs for updating existing STARTER resp. SCOUT installations
(please read detailed description)
 installableintegrated

SSP, SINAMICS G120 V4.7 SP3

  SSP_SINAMICS_G120_V4_7_SP3.zip (16,8 MB)

STARTER
from V4.4 1)

SCOUT
from V4.4 2)

STARTER
from V4.4 SP1

SCOUT
from V4.5

 You can find the suitable online help (optionally) here: 109483088 

With this SINAMICS Support Package, the SINAMICS / G120C / G120P / G120D series with firmware release V4.7 SP3 can be configured and commissioned using STARTER (observe restriction 1) ) or SCOUT (observe restriction 2) ).

Procedure for installing SSP:

  1. Download the attached ZIP file
  2. Unzip the ZIP file to a shared target directory on your hard disk.
    Please ensure that there are absolutely no spaces in the complete path names of this target directory.
  3. After unpacking, the shared directory must appear as follow:
    \...\01_Readme\
    \...\CD_1\
  4. Start the SSP setup program by calling it from /CD_1/SETUP.EXE.3)

The readme file contains important notes on how to use the tool.


3): Hint according the follow SSP Setup-notice: The SSP can not be installed because of an incorrect Windows operating system.
Please install the SSP via the actual version of the STARTER tool.

1): When configuring these power module types or the G120C, you must update to version STARTER V4.4 SP1. 

2): Only if this SINAMICS G120 SSP V4.7 SP3 is used/installed in context with SCOUT V4.4 or T-Config, please notice this link: 109482653 


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.