×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109483258, Entry date: 05/23/2016
(1)
Rate

Saving SCALANCE Configuration Data in an S7-1500

  • Entry
  • Associated product(s)
The SCALANCE switches of the XB-200 series, the W761 access point and the W72x client modules do not feature a C-PLUG slot for backing up configuration data. An alternative is to automatically save the configuration data in the controller.

To back up the configuration data or in case of device replacement, the user has the option to store the configuration on a storage medium (C-PLUG or configuration plug). The SCALANCE switches of the XB-200 series, the W761 access point and the W72x client modules do not feature a C-PLUG slot. A backup of the configuration data must be triggered manually and specifically using CLI or WBM. Automatic saving in the controller is an alternative to the C-PLUG.

Solution
The “SNMP” and “TFTP” function blocks were developed to implement the task – save the configuration data in the controller. They allow you to save and back up the configuration data (depending on the size) in one or more data blocks (DBs) (“upload”) and restore it due to maintenance or repair (“download”). The DBs are stored in the CPU’s load memory.
To do this, the application uses two protocols:

  • SNMP (Simple Network Management Protocol)
  • TFTP (Trivial File Transfer Protocol)


Figure 01

Variants
This application example provides two variants:

  • “Automatic” variant:
    Automatic “upload”/“download” of the configuration data of all network components supported and configured as a PROFINET IO device.
  • “Manual” variant:
    Manual, device-specific “upload”/“download” of the configuration data of one supported network component. An HMI can be used for operator control.

Advantages
The solution presented here offers the following advantages:

  • Central storage of the configuration data in the controller’s load memory.
  • Configuration data can be easily loaded back to the device in case of replacement or when restoring the original configuration.
  • Saves time and costs due to the use of existing mechanisms/protocols.
  • No additional hardware tools or devices required.

Documentation and Sample Project
  Documentation (1,5 MB) 
 Registrierung notwendig  Project for STEP 7 V15.1 (10,2 MB) 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.