×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109483368, Entry date: 06/13/2019
(1)
Rate

RFID basic examples: SIMATIC RF300 via RF120C

  • Entry
  • Associated product(s)
With the RF120C communication module you can integrate SIMATIC RF300 readers in a proprietary manner into a S7-1200 control system. The S7 block “ident blocks" or “ident profile" are used to control this configuration.

Task
A SIMATIC RF300 reader is to be integrated directly into a S7-1200 control system. Basic RFID functionalities are to be realized via the reader. 

Solution
The RF120C communication module was developed in order to connect the SIMATIC RFID reader directly to a S7 1200 control system. To control the readers the S7 "Ident blocks" program blocks are used.
The basic example for this solution is kept very simple. The focus in the description is on the basic steps for the configuration and programming of the automation solution. The figure below shows the structural configuration of the solution:
 


Documentation and example project for STEP 7 V15.1 with Technology object
 Registrierung notwendig  Documentation STEP 7 V15.1 (TO) (1,6 MB)
 Registrierung notwendig  STEP 7 V15.1 project for S7-1200 (TO) (1,6 MB)

Archive
Documentation and example project for STEP 7 V14 with Technology object
  Documentation STEP 7 V14 SP1 (TO) (1,7 MB)
 Registrierung notwendig  STEP 7 V14 SP1 project for S7-1200 (TO) (1010,0 KB)

Documentation and example project for STEP 7 V13
  Documentation STEP 7 V13 SP1 (1,0 MB)
 Registration required  STEP 7 V13 SP1 project for S7-1200 (4.2 MB)

Other basic examples for SIMATIC Ident
An overview of other basic examples with different hardware combinations can be found at the following link:
RFID basic examples


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.