×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109483556, Entry date: 04/28/2016
(0)
Rate

Which firewall settings do you have to make for SIMATIC B.Data V6.0 SP1?

  • Entry
  • Associated product(s)
If the network connection between single components is blocked by a firewall, problems might arise with the data transmission.

If single components of B.Data are installed on different computers, they are connected with each other via the network. During operation the data flow between the components is via this connection. If the network connection between single components is blocked by a firewall, problems might arise with the data transmission.

The document below shows how to configure the firewall to ensure perfect communication between the components of B.Data. This applies for operating systems Windows 7 / 8.1 and Windows Server 2008 / 2012.
 
 SIMATIC_B_Data_Firewall_Settings_en.pdf (1,2 MB)




Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.