×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109483774, Entry date: 09/05/2018
(5)
Rate

How many industrial monitors (IFPs) can you connect to one SIMATIC IPC?

  • Entry
  • Associated product(s)
You can connect 1 to 3 monitors to a SIMATIC IPC. The maximum distance is limited by the transmission technology implemented and can be up to 100m.

An industrial monitor consists of an input unit with touch sensor and an output unit for image output. The following explanations always apply for the complete device - input unit and output unit.

Abbreviations
The following abbreviations are used in this entry
 

 AbbreviationMeaning 
IFPIndustrial Flat Panel
IFP ETHIndustrial Flat Panel with Ethernet interface

Table 1

Note
Only monitors of the same type are permitted to be connected to a SIMATIC IPC; for example, an IFP with multitouch screen and another IFP with multitouch screen, or a Panel PC with resistive touch screen and another IFP with resistive touch screen.

Overview of the graphics interfaces of Box PCs and Panel PCs
 

 Box PCGraphics interfacesPanel PC Graphics interfaces

IPC227E
 
1x Display Port

IPC277E
 

1x Integrated display

1x Display Port


IPC427D
 

1x Display Port

1x DVI


IPC477D
 

1x Integrated display

1x Display Port or DVI


IPC427E
 
2x Display Port

IPC477E
 

1x Integrated display

2x Display Port


IPC627D
 

1x Display Port

1x DVI


IPC677D
 

1x Integrated display

1x Display Port

1x DVI

Table 2

Configurations up to 30m distance
The following table gives an overview of the maximum number of monitors you can connect to a SIMATIC IPC with a maximum distance of 30 meters (without Ethernet IFPs).

Overview of possible configurations of IPCs and monitors with distances of up to 30m 
 

SIMATIC IPCNumber of integrated monitorsMaximum number of IFPs with USB / DP / DVI interfaceMaximum number of monitorsBIOS, blue screens and advanced start options visible

227E

-11yes

427D

427E

627D

-22yes

277E

477D

112yes

477E

677D

123ja

Table 3

Restriction in Windows Embedded 7 - WES7 E
If you are using the operating system "Windows Embedded 7 - WES7 E" together with a multitouch monitor, then the touch sensor of the monitor must be switched to single-touch mode. Refer to the following FAQ response for single-touch mode in Entry ID: 109475464.

If you connect two monitors, both monitors must be in single-touch mode. Only the "duplicated" setting is permissible in the operating system.

A third monitor can only be used for display. You cannot operate via a third monitor. Therefore its use is not permitted.

Configurations with up to 100m distance
Overview of possible configurations of IPCs and monitors with distances of up to 100m distance
 

SIMATIC IPCNumber of integrated monitors

Maximum number of IFPs with USB / DP / DVI interface

(up to 30m)

Maximum number of IFPs with ETH / LAN interface

(up to 100m)

Maximum number of monitors *1)BIOS, blue screens and advanced start options visible

227E

427D

427E

627D

see

Table 3

see

Table 3

33no *2)

277E

477D

477E

677D

23yes

Table 4

Note
*1) The maximum number of all connected operator panels must not be exceeded.
*2) If IFP ETH monitors are connected via the ETH / LAN interface, then these monitors do not display any BIOS startup, blue screen messages or advanced start options. The reason for this is that an IFP ETH monitor can only display an image after the Ethernet driver has been enabled by Windows.

If BIOS startup, blue screen messages and advanced start options are to be displayed on an IFP ETH monitor, then the monitor has to be connected via the Display Port or the DVI interface on the IPC.

To operate 3 IFP ETH monitors on IPCs that only have 2 Ethernet interfaces you need an additional switch with at least 4 ports.

Together with IFP ETH (100m distance) you can only operate two IFP ETH displays in Clone mode. The third IFP ETH display or the panel of a Panel PC can only be operated in Extended mode. All three displays cannot be operated simultaneously in Clone mode.

Connection of more than 3 operator panels
If you connect more than 3 operator panels to a SIMATIC IPC, undefined states might occur if there is a power failure or the network connection is interrupted with IFP ETHs. For example, an IFP ETH displays no image but the touch screen can be operated.

Using a multitouch operator panel in single-touch mode
You can operate an MT operator panel either in MT or ST mode. In ST mode all touch events are reported as mouse events to the operating system. The operator panel acts as if it were equipped with an ST operator unit.

Switching to ST mode is necessary with operating systems that do not support MT, WES7 E, for example. Use the "Switch Touch Mode" tool to switch modes. The tool is included in "Panel Driver & Tools" version V1.1 and higher, or as a download in Entry ID109752279.

Please note that only a maximum of two operator panels can be operated when using an MT operator panel in ST mode. More information about operating a SIMATIC IPC with two monitors is available in Entry ID109475464.

Note in the case of power failure of a component or if the cable is disconnected
If the cable connection between a SIMATIC IPC and the connected operator panels has been temporarily disconnected, then check the assignment of the main and 2nd monitors as well as the touch function. If necessary, restart the SIMATIC IPC to restore the function of the operator panels.

Connection cables for operator panels with up to 5m distance
Connection cables are available in lengths of 3m and 5m for direct connection of a SIMATIC IPC with an operator panel via the DP, DVI-I and USB.

Connection cables up to 5m
 

Article numberDescription 
6AV7860-0DH30-0AA0SIMATIC IPC accessory, Display Port cable 3m, VESA-compatible
6AV7860-0DH50-0AA0SIMATIC IPC accessory, Display Port cable 5m, VESA-compatible
6AV7860-0BH30-0AA0SIMATIC Flat Panel Connection Cable Industrial Grade DVI-D 3m
6AV7860-0BH50-0AA0SIMATIC Flat Panel Connection Cable Industrial Grade DVI-D 5m
6AV7860-0CH30-0AA0SIMATIC Flat Panel Connection Cable Industrial Grade USB 3m
6AV7860-0CH50-0AA0SIMATIC Flat Panel Connection Cable Industrial Grade USB 5m

Table 5

Connection cables for operator panels with up to 30m distance
If you need a connection cable for a distance longer than 5m, connection cables up to 30m in length are available for DVI and USB connections. A connection via the DP interface is possible via a DP-to-DVI adapter cable and a DVI connection cable.

Connection cables up to 30m

Article numberDescription
6AV7860-1EX21-0AA1Cable set 10m, consisting of: DVI-D cable, CAT 5 cable USB send module
6AV7860-1EX21-5AA1Cable set 15m, consisting of: DVI-D cable, CAT 5 cable USB send module
6AV7860-1EX22-0AA1Cable set 20m, consisting of: DVI-D cable, CAT 5 cable USB send module
6AV7860-1EX23-0AA1Cable set 30m, consisting of: DVI-D cable, CAT 5 cable USB send module
6AV7860-1EX22-0BA1

Cable set 20m for IPC477C pro, consisting of: DVI-D cable angled 90°,

CAT 5 cable, USB sender module

6AV7671-1EX02-0AA0

PANEL PC USB INTERFACE SB103

6ES7648-3AF00-0XA0Display Port to DVI-D for onboard interfaces

Table 6