×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109485136, Entry date: 05/09/2019
(0)
Rate

DTM: SIPART PS2 PA - Profibus PA Profile 3.02 - SITRANS DTM 4.1

  • Entry
  • Associated product(s)

 

           

Engineering-Tool:

SITRANS DTM



 

Tool-Version:

V4.1

Supported Firmware:

>=V6.00.00

EDD-Version:

22.00.01

Order Number:

6DR5510-…..-…., 6DR5511-…..-….,

6DR5512-…..-…., 6DR5513-…..-….,

6DR5515-…..-…., 6DR5520-…..-….,

6DR5522-…..-…., 6DR5523-…..-….,

6DR5525-…..-…. 

 

Firmware-Version:

V6.00.00


This is the Device Type Manager (DTM) for SIPART PS2 Profibus PA for FDT Frame applications (e.g. PactWare) with SITRANS DTM.
For more information please check https://new.siemens.com/global/en/products/automation/process-instrumentation/positioners.html. 

SITRANS DTM - powered by EDDL
This installation file requires the software SITRANS DTM. SITRANS DTM has to be installed only once and can be downloaded from product support under the following links:
SITRANS DTM 3.1: https://support.automation.siemens.com/WW/view/en/53754140
SITRANS DTM 4.1: https://support.automation.siemens.com/WW/view/en/109484287
After the installation of SITRANS DTM ,any desired device DTM can be installed. To install the device DTM ,unzip it, then double-click on the .exe file and follow the instructions. More information about the installation can be found under the following link: /cs/document/61705616?caller=view&lc=en-WW

 Registrierung notwendig  SIPART_PS2_PA_DTM_FDT_22_01_00_03.zip (1,3 MB)

 



Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit