×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109485916, Entry date: 07/19/2016
(4)
Rate

PCS 7 Water Unit Template - Control of Biological Stage of a Wastewater Treatment Plant with Intermittent Operation

  • Entry
  • Associated product(s)
The PCS 7 Unit Template "Control of Biological Stage of a Wastewater Treatment Plant with Intermittent Operation" provides a template that comprises all typical components, theire open- and closed-loop control, the necessary logic as well as the visualization of a biological stage.

Task
The standardization of automation engineering for urban water management plants, such as water treatment, is a major challange. Different process steps and procedures, different equipment and flexibility in the plant configuration make the task even more difficult.



Solution
The application example "Control of Biological Stage of a Wastewater Treatment Plant with Intermittent Operation" is a unit template for water treatment plants, which can be integrated as a plant section in the most diverse urban water management plants. The unit template provides a template that comprises all typical components, their open- and closed-loop control, the necessary logic and interlocks as well as the visualization.

This application example presents a biological stage with which the energy consumption can be optimized by using an MPC (Model Predictive Control) controller. The construction is modular and based on standardized functions.

Its utilization offers the following advantages

  • A reduction of the knowledge necessary to develop the applications
  • A decrease of the configuration effort
  • Standardized structures

Procerement of the PCS 7 Unit Template
The PCS 7 project archive can be procured free of charge from your rigional Siemens Sales Partner.

Validity
This entry was created with SIMATIC PCS 7 V8.1 SP1 and CFC V8.1 SP1 Upd3, the procedure is valid for higher versions of SIMATIC PCS 7.


Further Informationen

Additional Keywords
water_wastewater, W&WW, WCMT, WMT, Water Library, MPC

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Requests and feedback
What do you want to do?