×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109736272, Entry date: 06/27/2016
(14)
Rate

Automatic synchronization of recipes on multiple panels

  • Entry
  • Associated product(s)
Two application examples on how to change recipe data on a panel and on how to synchronize these changes on all assigned panels.

Introduction
Recipes are used in many production facilities.
If in a plant, multiple production lines are operated, all of them using the same recipes, then changes to the recipes need to be done at all stations subsequently.

By two examples, the application illustrates how to synchronize recipe data on all related panels.

You therefore do not have to walk from station to station any longer to adjust modified recipe data.

The image shows the configured plant picture for example 1.
Example 1 can also be used for Basic Panels 2nd Generation.


Plant picture example 1

The image shows the configured plant picture for example 2.
Example 2 can be used, if you save recipe data centrally on an “Office-PC” via a network.


Plant picture example 2

The configuration was created with WinCC Comfort V13 SP1.

  Documentation (1,1 MB)

 Registrierung notwendig  Program example (14,4 MB)


Supplementary search terms
copy data, data records, data record, synchronous, adjust data, copy files, align data,


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.