×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109736504, Entry date: 07/10/2017
(2)
Rate

What are the relationships, differences and typical fields of application of input delay, pulse stretching and oversampling when acquiring fast digital signals?

  • Entry
  • Associated product(s)
Input delay, pulse stretching and oversampling are digital input module functions. These functions pre-process input signals before they are transferred to the CPU.

The functions are explained in detail in the manual of each module or system. The attached document shows the relationships and differences:

  Documentation (1,1 MB)

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.