×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109737290, Entry date: 05/31/2016
(0)
Rate

Setting up a secure VPN Connection between CP 1543-1 and SOFTNET Security Client

  • Entry
  • Associated product(s)
Setting up a secure connection between a PC of a service technician and a SIMATIC-Station over the Internet with the aid of CP 1543-1 and SOFTNET Security Client.

Due to increased networking through Ethernet, remote diagnostics and/or remote maintenance are of great importance in modern automation systems. Today's Internet access mechanisms (wireless, broadband) and the security components from Siemens are an ideal combination for industrial remote communication.
A VPN tunnel is the typical way to establish a secure connection between two networks (e.g., automation networks or individual devices).
A VPN is a virtual, logical private network based on a publicly accessible infrastructure. Only communication partners that belong to this private network can communicate with each other and exchange information and data. 

This application shows the user how to establish a secure connection between two networks over the Internet with the aid of Siemens' Security Products portfolio.

Solution
The security modules CP 1543-1 and SOFTNET Security Client are used to implement the task.
 


Image 01
 
Characteristics
The solution described in this application has the following characteristics:
  • VPN tunnel for flexible access to the automation cell - possible, for example, for a service employee.
  • Controlled, encrypted data traffic between CP 1543-1  and SOFTNET Security Client.
  • Integrated network diagnostics via SNMP or Syslog.
  • The firewall, VPN server and communication settings are made directly in the CP 1543-1; the security functions are integrated in the communications processor.
  • Protection of the SIMATIC controller without an additional security module.
  • Secure lower-level networks can be operated via additional Ethernet/PROFINET interfaces, realized by the CPU or additional CPs.

Download
 Registrierung notwendig  Documentation (998,0 KB) 

Further Information 
Getting Started with Industrial Remote Communication
All-Round protection with Industrial Security


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.