×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109737292, Entry date: 03/06/2017
(4)
Rate

SINAMICS G: Telegram Extension of a Position-Controlled Drive with SIMATIC S7-1500 (TO)

  • Entry
  • Associated product(s)
Option of extending the telegram when using the “Positioning axis” technology object

SIMATIC S7-1500 CPUs support the connection of PROFIdrive-capable drives via PROFINET or PROFIBUS as a speed axis or positioning axis. To do this, a technology object communicating with the drive via defined standard telegrams is configured in the control program. In addition to the already existing standard telegram, additional parameter values shall be transmitted between the controller and the drive.


Solution
In this application example, a SINAMICS G120 is operated as position-controlled drive. A telegram extension is used in order to ensure that additional parameter values can be exchanged between the controller and the drive.

Download

  Documentation (1,7 MB)
 Registrierung notwendig  STEP 7 TIA Portal V14 Project (420,3 KB)


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit