×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109738387, Entry date: 07/30/2020
(67)
Rate

SINAMICS V-ASSISTANT Commissioning tool

  • Entry
  • Associated product(s)
The latest version of SINAMICS V-ASSISTANT commissioning tool for the device SINAMICS V90 is provided here.

Description

Support product types:

  • SINAMICS V90 with Pulse train, USS/Modbus interface (V90 PTI)
  • SINAMICS V90 with PROFINET (V90 PN)
Use of SINAMICS V-ASSISTANT is free of charge and does not require a license key to be entered.
The firmware version can be checked via parameter r29018.


SINAMICS V-ASSISTANT V1.06.02

Variants

Article number

Support Firmware

SINAMICS V90 PN

6SL3210-5Fxxx-xxFx

V1.04.01, V1.03.00, V1.02.0x and all lower versions

SINAMICS V90 PTI

6SL3210-5Fxxx-xxAx

V1.11.01, V1.10.00, V1.09.01 and all lower versions

What is new:

  • Support referencign with reversing cams in "Reference cam (signal REF) and encoder zero mark" and "Encoder zero mark only"
    • Open new parameter p29239 to activate reversing cam
  • Support cyclical communication of customized PZD 13 ~ 14 for EPos reference point coordinate value 
    • Open new paramter p29152 to activate customized PZD 13~14
  • Support DI/DO controlled by PROFINET via telegram 111
    • Add new value for p29150(User defined PZD receive): p29150 = 3
    • Add new value for p29330 (DO_1) and p29331 (DO_2): p29330, p29331 = 16, 17 
  • Open new parameter p1433: set the speed controller reference model natural frequency based on mechanism manually.
  • Open new parameter p1981: help to set the maximum distance manually when carrying out the pole position identification routine for the motor with incremental encoder.

Notice:

SINAMICS V-Assistant support only 64-bit operating system from V1.06.02.

Language packages

From V-ASSISTANT software version V1.05, the supported language packages shall be installed independently. The English and Chinese are integrated in the V-ASSISTANT installation package.

Language

Download

English

Integrated in the installation package

Chinese

Integrated in the installation package

German

 Registrierung notwendig  lang_deu_v10602.zip (34,4 MB)

French

 Registrierung notwendig  lang_fra_v10602.zip (35,5 MB)

Italian

 Registrierung notwendig  lang_ita_v10602.zip (35,0 MB)

Spanish

 Registrierung notwendig  lang_esp_v10602.zip (35,1 MB)

Turkish*

 Registrierung notwendig  lang_trk_v10602.zip (35,6 MB)

Portuguese*

 Registrierung notwendig  lang_ptb_v10602.zip (35,7 MB)

______________________________________________________________________________________________

Here you can find the previous version of SINAMICS V-ASSISTANT


SINAMICS V-ASSISTANT V1.06

Variants

Article number

Support Firmware

SINAMICS V90 PN

6SL3210-5Fxxx-xxFx

V1.03.00, V1.02.01, V1.02.00 and all lower versions

SINAMICS V90 PTI

6SL3210-5Fxxx-xxAx

V1.11.01, V1.10.00, V1.09.01 and all lower versions


What is new:

  • Supports new SINAMICS V90 PTI firmware version V1.11 and the following new functions are supported by V-Assistant V1.06
  • Supports V90 PTI new control mode: Fast PTI mode
  • Supports new I/O configuration under Fast PTI mode
  • Opens new tuning paramter p1433 and trace parameter p2521[2] and p2522[2].


SINAMICS V-ASSISTANT V1.05.05

Variants

Article number

Support Firmware

SINAMICS V90 PN

6SL3210-5Fxxx-xxFx

V1.03.00, V1.02.01, V1.02.00 and all lower versions

SINAMICS V90 PTI

6SL3210-5Fxxx-xxAx

V1.10.00, V1.09.01, V1.09.00 and all lower versions


What is new:

  • Supports new SINAMICS V90 PN firmware version V1.03 and SINAMICS V90 PTI firmware version V1.10. The following new functions are supported by V-Assistant v1.05.05.
  • Support Supplementary telegram 750 for torque control.
  • Support Feedforward setting adaption to motor types.

Language packages

The supported language packages SINAMICS-V-ASSISTANT V1.05.05 are the same as previous version. Starting from V-ASSISTANT software version V1.05, the supported language packages shall be installed independently. The language package contains the text of online help and HMI. The English and Chinese are integrated in the V-ASSISTANT installation package.

Language

Download

English

Integrated in the installation package

Chinese

Integrated in the installation package

German

 Registrierung notwendig  lang_German_1.0505.zip (30,6 MB) 

French

 Registrierung notwendig  lang_French_1.0505.zip (31,8 MB)

Italian

 Registrierung notwendig  lang_Italian_1.0505.zip (31,2 MB)

Spanish

 Registrierung notwendig  lang_Spanish_1.0505.zip (31,4 MB)

Turkish*

 Registrierung notwendig  lang_Turkey_1.0505.zip (31,9 MB)

Portuguese*

 Registrierung notwendig  lang_Portugal_1.0505.zip (31,9 MB)


How to install SNAMICS V-ASSISTANT

  1. Download the attached ZIP file

  2. Unpack the ZIP file into a target directory on your hard disk.

  3. Start the installation program by double-clicking the “Setup.exe” file.

  4. Finish the installation according to the instructions on the screen.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.