×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109738589, Entry date: 07/08/2016
(0)
Rate

Sales and Delivery Release for SIMATIC WinCC/PerformanceMonitor V 7.4

  • Entry
  • Associated product(s)
WinCC/PerformanceMonitor V 7.4 - Production analysis and optimization on the basis of individual key performance indicators


The WinCC/PerformanceMonitor enables a flexible calculation and powerful analysis of plant-specific key performance indicators (KPIs). These figures are the basis to develop optimization potentials to increase the productivity.

Note:
Please note that the SIMATIC WinCC/PerformanceMonitor V7.4 requires SIMATIC WinCC V7.4 or higher updates and service packs (see entry IDs:109483726


 1. The Functions at a Glance

The calculation of performance figures is based on operands which are formed of already configured WinCC variables. A combination with collateral values enables more accurate production contexts to be emphasized, e.g. quality depending on the supplier. The performance figures and the production contexts are assigned to the plant subsections. The calculation formula used can be developed quickly and easily in WinCC. The calculated data by PerformanceMonitor can be stored in Process Historian.

The analysis of the performance figures and their operands is possible at any time in the WinCC system. Performance figures, if required with their collateral values, can be clearly represented and compared in bar charts. In addition, the input values of each performance figure can be displayed via an integrated analysis function (drill-down). The Gantt diagram displays the chronology of the time-based operands. A spreadsheet can be used to list and, if necessary, correct the archived values at a later date. Cyclically or variables triggered online calculated performance figures can be written to WinCC tags for further processing in WinCC, e.g. for indication in WinCC screens.

The PerformanceMonitor can be combined with the WebNavigator for distribution in the Internet and the Information Server for reporting.  The integration in WinCC ensures fast configuration and full transparency of all machine and plant data as basis for optimization of the plant productivity. 

  • The WinCC/PerformanceMonitor can be installed on a WinCC Single Station, WinCC Server or WinCC Client project (RT 128 license) and consists of an Engineering Client as well as a Runtime User Interface.
  • The WinCC/ PerformanceMonitor provide ActiveX control elements for inclusion in WinCC screens.
  • PerformanceControl: Bar chart for representation of the performance figures in relation to context values with indication of the relevant operands for cause analysis.
  • Gantt diagram: Horizontal progress display of time-based operands
  • TableControl: Tabular list of the operands with a subsequent correction option.
  • With the aid of the integrated configuration environment operands are calculated on the basis of variables, which are used for the performance figure calculation at the time of the evaluation.
  • If the WinCC/WebNavigator is used, the controls of the WinCC/ PerformanceMonitor are available for analysis via the Internet or Intranet
  • The SIMATIC Information Server can be used for plant-specific web-based reports (pre-defined, expandable reports).
  • The archived values (operands, context) form the basis for the analysis and are additional license-relevant via one-by-one licensing.

    Management and quality assurance benefits

          Full transparency of the machine equipment as basis for optimization of the plant productivity.

    • Capturing of downtimes, localization of the causes of downtimes and monitoring of the equipment efficiency.
    • Decision finding on the basis of performance indicators.
    • Globally available reports of the Information Server for different user groups
    • Capturing of downtimes, localization of the causes and reasons for the downtimes and monitoring of the equipment efficiency.
    • Identification of production correlations due to the combination of the performance figures with collateral values, e.g. the material used.

        Service and Maintenance

            Support from performance figure calculations triggered cyclically and via process events:

      • Standardization of new plants by the definition of controller-based status information for performance figure calculation
      • Individual pinpointed analysis by plant-specific performance figures.
      • Weak point analysis in production processes and detection of unwanted process characteristics. 
      • Cause analysis by investigation of the calculation basis "drilldown to operands".
      • Identification of events which will result in cost-intensive failures.

        Line management and operator

            The operator is always optimally informed via the graphically displayed performance figures. 

        • Subsequent changes of the archived input values.
        • Continuous information of the operator due to integration in the WinCC user interface.
        • Alarming in the case of limit value violation and trend recording with cyclical performance figure calculation.
        • Quick identification of weak points in the process with cyclical performance figure calculation.

          WinCC Engineering

          • Subsequent changing of the archived input values.
          • Fast configuration of the WinCC control views with WinCC and web-based reports with the Information Server.
          • Minimization of the networking effort due to the use of the WinCC infrastructure in the local network and the Internet.
          • Minimum training period and simple configuration due to the use of known tools for the user interface and the reports (WinCC, SIMATIC Information Server)
          • Minimum configuration work due to the Type Instance Concept
          • Minimum administration work due to the use of the WinCC infrastructure in the local network and the Internet.

          • Engineering fully intehgrated in WinCC Configuration Studio.

            Highlights  

                Creation of performance figures by the WinCC engineer with subsequent use by all user groups of the production facility on WinCC stations or Internet clients.    

              Application area 

                  The PerformanceMonitor serves all user groups, from the application engineer up to evaluation by the management. With the application environment integrated in WinCC the engineer can create the individual formula for         the calculation of the performance figures. The management can use the web-based reporting on standard computers without any further installation. The maintenance department can use the web client of the WebNavigator     for analysis with bar charts (performance); progress displays (Gantt) and tabular control. The representation of the performance figures with WinCC standard means on the on-site user interfaces keeps the machine operator     up-to-date. The maintenance engineer can use the WinCC Client, the web client of the WinCC/WebNavigator, to analyse the plant from his workplace. Management always has access to web-based reports on standard         computers without any further installation. 

                Function 

                • Structuring of the production plant into equipment, as central constituents for the evaluations.
                • Use of structured variables in order to use machine status models.
                • WinCC Variables are consolidated into an operand by means of formulae.
                • Calculated operands are stored in an archive.
                • Archived operands are used as input values for performance figure calculation.
                • Bar charts for the analysis of performance figures and the investigation of causes (drilldown). The input values (operands) of the performance figures can be displayed for this purpose

                    Tabular representation of all operands (input values), progress diagram (Gantt chart), time-based operands. Cyclical or event-triggered calculation results are written to WinCC variables. WinCC runtime, alarm logging and     trend logging can use the cyclically calculated values. The evaluation and display of the information from the database is available to every WinCC station. The reports of the Information Server can be displayed on                     independent PC workstations.   

                  Product overview


                    The basic package consists of the configuration environment, the runtime controls (bars, Gantt chart, table) and the license to archive 30 values. The archived values (operands, context) form the basis for the analysis. If more values must be archived they can be increased in steps of 30, 100, 300 or 1000 archive values (additive).

                    Compared to SIMATIC WinCC/PerformanceMonitor V7.3, SIMATIC WinCCV/PerformanceMonitor V7.4 includes the following changes to the range of functions in addition to consolidation of the WinCC updates that have been published by then:

                    Engineering Enhancements:

                    • Integration into WinCC Configuration Studio (VBA is also possible)
                    • Import / Export to CSV and Excel
                    • Information which KPIs, operands and contexts are in use
                    • Anchor point can be set by a tag

                    Graphical Enhancements:

                    • Capability to display in one row all the info related to one  equipment in the PerformanceGanttControl
                    • Different layouts of bars inside PerformanceViewControl

                    Licensing:

                    Structured Operands are now counted only as 1 Archived tag each, regardless how many values it can assume.

                     
                    2. System requirements

                    The software and hardware requirements for WinCC/PerformanceMonitor V7.4 are the same as for WinCC V7.4 plus additional CPU speed and RAM according with the quantity of ArchiveTags used in the application developed. The same operating systems of for WinCC V7. 4 are supported (see entry ID: 109483726 )



                    3. Licensing

                    The license is valid for each single-user or server. No license is required on the WinCC Clients. 

                    The following license is available:

                      SIMATIC WinCC/PerformanceMonitor V7.4

                      4. Delivery Scope and Ordering Data The delivery of the WinCC/PerformanceMonitor is comprised of the WinCC/PerformanceMonitor V7.4 CD, a USB stick and a Certificate of License. The documentation in five languages is contained on the CD



                      Ordering Data

                      Order Number

                      WinCC/PerformanceMonitor V7.4  Basic Package incl. 30 PerformanceMonitor Archives

                      6AV6372-2DG07-4AA0

                      30 PerformanceMonitor ArchiveTags (additive)

                      6AV6372-2CG20-0BA0

                      100 PerformanceMonitor ArchiveTags (additive)

                      6AV6372-2CG20-0CA0

                       300 PerformanceMonitor ArchiveTags (additive)

                      6AV6372-2CG20-0DA0

                      1000 PerformanceMonitor archive ArchiveTags (additive)

                      6AV6372-2CG20-0EA0

                      WinCC PerformanceMonitor Upgrade
                      Upgrade WinCC PerformanceMonitor 7.2 to WinCC PerformanceMonitor 7.3

                      6AV6372-2DG87-3AA0

                       


                      The ordering data for WinCC V7.4 can be found in the delivery release with the entry ID: 109483726 



                      Security information
                      In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
                      https://www.siemens.com/cybersecurity#Ouraspiration.