×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109738680, Entry date: 10/18/2016
(0)
Rate

Security Updates 10/2016 for SIMATIC PCS 7 V8.0+SP2 and SIMATIC PCS 7 V8.0+SP2 ASIA

  • Entry
  • Associated product(s)
The installation of the security updates referenced below is recommended for all ES/OS stations as well as for the system components SIMATIC BATCH, SIMATIC Route Control and OpenPCS 7 of the SIMATIC PCS 7 V8.0+SP2 process control system. Further information on the individual updates and installation instructions are provided in the readme files which are supplied with the installation software.

Note:
To be able to load configuration changes it is necessary that the software versions of all target systems are identical. It is thus mandatory that the Security Updates referenced below are installed on all the affected SIMATIC PCS 7 Industrial Workstations.

Installation files

Update 13 for SIMATIC WinCC V7.2 and SIMATIC WinCC V7.2 ASIA
 (core component in all ES/OS stations of the SIMATIC PCS 7 V8.0+SP2 process control system)

Update 17 for SIMATIC BATCH V8.0+SP1

    Update 6 for SIMATIC Route Control V8.0+SP1

    Update 8 for SIMATIC PCS 7 Open/PCS 7 V8.0+SP1

    Security information
    In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
    https://www.siemens.com/cybersecurity#Ouraspiration.
    Rate entry
    no rating
    Requests and feedback
    What do you want to do?
    Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.