×
Siemens Industry Online Support
Siemens AG
Entry type: Product note, Entry ID: 109739352, Entry date: 07/21/2016
(0)
Rate

Sales and Delivery Release for SIMATIC WinCC/Event Notifier V7.4

  • Entry
  • Associated product(s)
The new WinCC option SIMATIC WinCC/Event Notifier V7.4 is herewith released for delivery. Please note that the SIMATIC WinCC/Event Notifier V7.4 requires SIMATIC WinCC V7.4, or higher updates (see entry ID: 109483726)

The new WinCC option SIMATIC  WinCC/Event Notifier V7.4 is herewith released for delivery.

Please note that the SIMATIC WinCC/Event Notifier V7.4 requires SIMATIC WinCC V7.4, or higher updates (see entry IDs: 
109483726)



1. The Functions at a Glance

The option SIMATIC WinCC/Event Notifier provides a calender-based user interface in the style of Microsoft Office, for easy and safe planning of notifications for selected persons in defined time slots. The option consists of a Calendar Control plus editors with which notifications as well as contacts can be configured and managed as potential targets for notification. During the configuration the notifications are assigned to directly selectable events in the WinCC signaling system, contacts can be recruited from the WinCC UserAdministrator even during runtime. Finally, a Communication Service Editor enables the creation of the communication service via e-mail service at the time of configuration, i.e. the notifications triggered in the WinCC signaling system in the case of a specific event are always dispatched via e-mail. However, the e-mail can also be routed as SMS to a mobile phone via Provider Gateway, if the relevant contact has been suitably established and the person in question has enabled this service for himself with his provider. If several persons or groups of persons are installed in Calendar Control in parallel in the same time slot, escalation stages can be implemented by the assignment of different escalation times (= reaction time before the notification). 

    Event Notifier editors

    The Event Notifier provides editors for the configuration and administration of notifications and contacts. A Communication Service Editor enables the configuration of the e-mail service
     
    Calendar Control

    The Calendar Control is configured in the Graphics Designer and can be made dynamic in WinCC using all WinCC standard mechanisms such as tag connections, VBS, C, direct connections or dynamic dialogs.
     
     Supported functions       

    -
    Access protection via WinCC UserAdministrator
    - Configuration of the E-Mail service for notifications
    - Configuration of notifications including support of the WinCC runtime languages by connection to the WinCC alarm system
    - Planing of the notification of selected persons in defined time slots in a way similar to the Microsoft Office calender
    - Dragging and dropping of contacts from the WinCC UserAdministrator as potential targets for notifications
    - Different calenders
    - User-defined calender views
    - Server Client, Redundancy and WebNavigator
     

    2. System requirements

    The software and hardware requirements for WinCC/Event Notifier V7.4 are the same as are the same as for WinCC V7.4. The same operating systems as for WinCC V7.4 are supported (see entry ID: 109483726)

    3. Licensing

    The license is valid for each single-user or server. No license is required on the WinCC Clients. 

    The following license is available:

      SIMATIC WinCC/Event Notifier 7.4

      4. Quantity structure

      There are no quantity limitations with regard to the number of contacts.
      Due to the connection to the WinCC User Admin the number of contacts is limited to max. 128.

      5. Delivery Scope and Ordering Data

      The delivery of the WinCC/Event Notifier is comprised of the WinCC/Calendar Options V7.4 CD, a USB stick and a Certificate of License. The documentation in five languages is contained on the CD.
       

      Product Name

      Order Number

      SIMATIC WinCC/Event Notifier V7.4

      6AV6372-1DD07-4AX0

      SIMATIC WinCC/Calendar Options Upgrade V7.x -> V7.4 (*

      6AV6372-1DC07-4AX3

       


      (* The license upgrade (6AV6372-1DC07-4AX3) is valid for both programs of the Calender options (Calendar Scheduler and Event Notifier). With the purchased upgrade license the upgrade can only be applied to one of the programs (Calendar Scheduler or Event Notifier) on each server. If you require upgrades for both programs and for several servers, you must purchase the corresponding number of upgrades.    

      The ordering data for WinCC V7.4 can be found in the delivery release with the entry ID 109483726

      Security information
      In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
      http://www.siemens.com/industrialsecurity.