×
Siemens Industry Online Support
Siemens AG
Type de contribution : Exemple d’application ID de la contribution : 109739384, Date de la contribution : 07/02/2017
(2)
Évaluer

SIMATIC IPC – Protection against power failures

  • Contribution
  • Concerne le/les produits(s)
Measures for the protection of an IPC against power failures and resulting data loss.

In a production hall, there is a production machine, an electric drive motor and an industrial PC (IPC) to control and monitor the production process. The IPC, the production machine and the electric motor are supplied via the same power grid. During the switch-on process, the motor requires a high start-up current. This often causes voltage fluctuations in the electric supply grid and
an insufficient power supply of the IPC. As a result, malfunctions and data loss may occur.
Therefore, the energy supply of the IPC should be stabilized with a suitable power supply. This way, data loss resulting from an instable supply system can be prevented. The IPC shall continue to work independently in the event of a power failure of several seconds. If the power failure lasts longer, the IPC shall shut down by itself


Protection against power failures

This application example covers the protection of a SIMATIC IPC against voltage fluctuations and power failures

Download
  SIMATIC IPC - Protection against power failures (1,1 MB) 

Additional keywords
USV, UPS, SV, PSU, power, voltage, failure, protection, buffer

Notes relatives à la sécurité
La protection des installations, systèmes, machines et réseaux contre les cyber-menaces nécessite la réalisation (et le maintien continu) d'un concept global de sécurité IT à la pointe de la technique. Les produits et solutions Siemens ne constituent qu'un élément d'un tel concept. Pour plus d’informations sur la cyber-sécurité, rendez-vous sur
https://www.siemens.com/cybersecurity#Ouraspiration.
Aide pour la statistique
Cette fonction permet de délivrer les identifiants des résultats de la recherche selon la quantité souhaitée (format .txt).

Générer une liste
Copier l'URL
Afficher cette page dans le nouveau design
Poste de commande mySupport