×
Siemens Industry Online Support
Siemens AG
Type de contribution : Informations sur le produit ID de la contribution : 109739471, Date de la contribution : 30/09/2016
(15)
Évaluer

Delivery Release of TIA Portal V14

  • Contribution
  • Concerne le/les produits(s)
Delivery release of TIA Portal V14: Your gateway to automation in the Digital Enterprise

Your gateway to automation in the Digital Enterprise

TIA Portal V14 offers a large variety of new functions for existing products


In addition, new TIA Portal options as well as new STEP7 and WinCC options are now available.

Overview of the new options in V14




TIA Portal V14 options


Engineering options

TIA Portal Multiuser Engineering

TIA Portal Multiuser Engineering enables multiple users to simultaneously work on a single project.
As a result, configuration times are significantly reduced and projects can be commissioned quicker.

The basic principle:

  • Project management is performed by a stand-alone server application. The server application can be installed independent of a TIA Portal

or

Project management is located on a server. The server can be installed independent of a TIA Portal.

  • Different users work in local sessions based on the projects managed by the server.
  • Users work independently in local sessions. Changes made by other editors are displayed and can be transferred.
  • Changes from the local sessions are transferred by checking them into the server project.

TIA Portal Teamcenter Gateway

The Teamcenter Gateway enables you to save and manage TIA Portal projects and global libraries in Teamcenter. Operator control is integrated into the TIA Portal.

TIA Portal Cloud Connector

The TIA Portal Cloud Connector provides access to local PC interfaces and connected SIMATIC hardware in the TIA Portal Engineering while the engineering itself is performed via Remote Desktop in a private cloud

SIMATIC Energy Suite

As an integrated option for the TIA Portal, SIMATIC Energy Suite directly links energy management and automation for the first time and thereby creates energy transparency in the production system. In addition, simplified programming of energy-measuring components significantly reduces the configuration work. see also

  • Integrated and intuitive configuration of the energy management
  • Automatic generation of the PLC energy program for S7-1500
  • Archiving on WinCC Runtime Professional or PLC-internal SIMATIC memory card
  • Seamless connection to SIMATIC Energy Manager PRO

SIMATIC PLCSIM Advanced

SIMATIC PLCSIM Advanced enables you to create virtual controllers for simulating S7-1500 and ET 200SP controllers and provides extensive simulation of functions. Compared to the standard S7-PLCSIM, PLCSIM Advanced offers the following additional functions:

  • API for connection to co-simulations
  • Multiple, distributed instances possible
  • Web server and OPC UA access

SIMATIC ODK 1500S

ODK 1500S enables the development of function libraries with the high-level languages C/C++ for SIMATIC S7-1500 PLCs that support ODK. These function libraries can be loaded and executed directly from the user program. S7-1500 PLCs that support ODK:

  • S7-1500 Software Controller (CPU 1507S (F))
  • ET 200SP Open Controller (CPU 1515SP PC (F))
  • S7-1500 Advanced Controller (CPU 1518(F)-4 PN/DP ODK)

SIMATIC Target 1500S™ for Simulink®

Target 1500S is an add-on for Simulink from MathWorks. It enables the
integration of Simulink models directly in the program cycle of an S7-1500 PLC that supports ODK.

  • Enables model-based development with MATLAB® and Simulink for SIMATIC controllers
  • Seamless integration into Simulink as a "System" target file
  • No C/C++ or ODK expertise required
  • Support for the Simulink external mode for immediate monitoring and control of model parameters in the controller from within Simulink
  • The generated code runs on CPU 1507S(F) V2.0, CPU 1515SP PC (F) V2.0 and CPU 1518(F)-4 PN/DP ODK.

SIMATIC Visualization Architect

SIMATIC Visualization Architect (SiVArc) enables simple, fast, flexible and automated creation of HMI contents based on the STEP 7 user program.

  • Supported HMI devices:
  • Comfort Panel, Mobile Panel 2ndGen, WinCC RT Professional, WinCC RT Advanced
  • Supported HMI objects:
  • Screens, text lists, power tags, captions, buttons, I/O fields, symbolic I/O fields, graphic I/O fields, switches, round buttons
  • Configuration using rule editors
  • Templates are managed using libraries


Runtime options

The following new options are offered exclusively as runtime options for TIA Portal V14.
The ProDiag and OPC UA S7-1500 products are already integrated into the existing STEP 7 and WinCC products and only need to be licensed for use with real hardware. Unlike engineering options, the runtime options are independent of the version.

SIMATIC ProDiag

Selective and fast machine and plant diagnostics for SIMATIC S7-1500 and SIMATIC HMI:

  • Central time stamping of fault alarms for specific cycles
  • Automatic generation of the monitoring logic and alarm calls
  • Automatic update of the SIMATIC HMI for changes to the alarm configuration for three languages
  • HMI systems need not exit runtime mode for changes
  • Directly available in the language editors LAD, FBD, SCL and STL
  • Supervisions can be retro-configured to F-blocks and protected blocks
  • Central specification of the alarm structure for each project
  • Alarm texts are automatically derived from the information in the project
  • Easy visualization on the HMI using pre-made controls

SIMATIC OPC UA S7-1500

The OPC UA S7-1500 option enables easy connection of any third-party device to the S7-1500 via the OPC UA server integrated in the S7-1500 CPU:

  • OPC UA server directly in the S7-1500
  • OPC UA data access, read/write, subscription to value changes
  • Security
  • XML export for offline configuration of OPC UA clients


SIMATIC Energy Suite S7-1500

The SIMATIC Energy Suite engineering comes with 10 energy objects. Additional energy objects can be added with runtime packages.

WinCC/WebUX

WinCC/WebUX for WinCC Professional enables monitoring of plant processes and, if required, controlling them over the Internet or intranet by means of mobile HMI devices. The software provides a visualization solution suitable for HTML5 and browsers that support SVG regardless of the operating system – without any engineering work.
WinCC/WebUX

Ordering data


The products with article numbers (order numbers) are listed in the attached file:

 Registrierung notwendig  tia_portal_v14_orderlist.xls (40,0 KB)


Trial software download

Trial versions of the TIA Portal products STEP 7, STEP 7 Safety, WinCC and Startdrive can be downloaded and tested using this entry: 109740201


 

Notes relatives à la sécurité
La protection des installations, systèmes, machines et réseaux contre les cyber-menaces nécessite la réalisation (et le maintien continu) d'un concept global de sécurité IT à la pointe de la technique. Les produits et solutions Siemens ne constituent qu'un élément d'un tel concept. Pour plus d’informations sur la cyber-sécurité, rendez-vous sur
https://www.siemens.com/cybersecurity#Ouraspiration.
Aide pour la statistique
Cette fonction permet de délivrer les identifiants des résultats de la recherche selon la quantité souhaitée (format .txt).

Générer une liste
Copier l'URL
Afficher cette page dans le nouveau design
Poste de commande mySupport